Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging two 3.7v Li-Ion Cells
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 287 subscribers
  • Views 6026 views
  • Users 0 members are here
  • series
  • lithium
  • 7.4
  • 3.7
  • charger
Related

Charging two 3.7v Li-Ion Cells

e14 Contributor
e14 Contributor over 11 years ago

So for a portable project, I will be using two lithium ion 2200mah 3.7v batteries in series to give me 7.4v. I have a USB powered 3.7v Lithium Ion charger found here https://www.adafruit.com/products/1905 . How could I charge both the batteries in parallel and then use them in series for 7.4v?

 

All help is greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to dougw +2
    I see some problems with this idea - if one battery is at a significantly different state of charge and thus voltage form the other (and this happens as the batteries age) then a huge current will flow…
  • Kilohercas
    Kilohercas over 11 years ago in reply to derkarhu +1
    You can also make very expensive circuit for battery charging, with CCCV push/pull 3A converters, just treat them as capacitors http://cds.linear.com/docs/en/datasheet/8052ff.pdf Super-capacitors are equivalent…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Please note that I am using the Adafruit Li Ion 3.7v charger, which safely charges the cells. I have decided that it is safer to just charge the 3.7v cells in parallel, which I have already tested and confirmed, and then boost the voltage to what I need for my project, using a 7.4v switching regulator.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    Please note that I am using the Adafruit Li Ion 3.7v charger, which safely charges the cells. I have decided that it is safer to just charge the 3.7v cells in parallel, which I have already tested and confirmed, and then boost the voltage to what I need for my project, using a 7.4v switching regulator.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • derkarhu
    derkarhu over 11 years ago in reply to e14 Contributor

    Whatever works for you. ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Kilohercas
    Kilohercas over 11 years ago in reply to derkarhu

    You can also make very expensive circuit for battery charging, with CCCV push/pull 3A converters, just treat them as capacitors image

    http://cds.linear.com/docs/en/datasheet/8052ff.pdf

     

    image

    Super-capacitors are equivalent to batteries in this circuit