Power & Energy
  • Technologies
  • More
Power & Energy
Forum Lipo to Li-Ion Upgrade swap
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 282 subscribers
  • Views 6737 views
  • Users 0 members are here
Related

Lipo to Li-Ion Upgrade swap

o.thornwall
o.thornwall over 6 years ago

Hello All,

The photo attached is of a 3.7v 870mAH Lipo battery. It has a circuit protection PCB (of some kind) attached to it.

 

My goal is to replace this Batt with a Li Ion Batt of the same Voltage but with 3000 mAH of currant.

 

So my question is: Should I remove this protection device and add it to the Li Ion Batt, or should or could I

 

calculate or obtain a new protection device (some how) for the larger mAH battery ?

 

Do I sound like I'm uneducated in the field of electronic ? You'd be right. But I do have some electrical experiencs

 

and I can soldier.

 

Any video explaining this lesson would be greatly appreciated.

 

Thornwall

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +5
    Hi Oscar, Neither : ) You can buy a battery with built-in protection circuit and wires on the end, all pre-assembled reasonably well and partially safe (to a limited extent). The ones without the circuit…
  • o.thornwall
    o.thornwall over 6 years ago in reply to shabaz +2
    1. So Shabaz, your saying the PCB attached to the Batt is a "Protection circuit" device ? 2. How would I discover the exact specification of the "Protection" PCB ? 3. Where would I find a Li-Ion Batt with…
  • genebren
    genebren over 6 years ago in reply to o.thornwall +2
    Thorn, Here is an example of a Li-Ion battery that will meet your specifications. Beware, there are a lot of fake batteries and/or claims out there. Buy from a reputable seller. (Note: these are listed…
Parents
  • shabaz
    shabaz over 6 years ago

    Hi Oscar,

     

    Neither : ) You can buy a battery with built-in protection circuit and wires on the end, all pre-assembled reasonably well and partially safe (to a limited extent).

    The ones without the circuit are intended for specialist use usually (such as to be assembled into a battery pack with specialist equipment).

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 6 years ago

    Hi Oscar,

     

    Neither : ) You can buy a battery with built-in protection circuit and wires on the end, all pre-assembled reasonably well and partially safe (to a limited extent).

    The ones without the circuit are intended for specialist use usually (such as to be assembled into a battery pack with specialist equipment).

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Children
  • o.thornwall
    o.thornwall over 6 years ago in reply to shabaz

    1. So Shabaz, your saying the PCB attached to the Batt is a "Protection circuit" device ?

     

    2. How would I discover the exact specification of the "Protection"  PCB ?

     

    3. Where would I find a Li-Ion Batt with the maH spec I want, with the correct spec "Protection circuit" PCB ?

     

    I've looked  around alot and havent seen any Li-Ion batts of 3.7v with any "Protection circuit" PCB's attached and for sale ?

     

    Thorn

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 6 years ago in reply to o.thornwall

    Thorn,

     

    Here is an example of a Li-Ion battery that will meet your specifications.  Beware, there are a lot of fake batteries and/or claims out there.  Buy from a reputable seller.  (Note: these are listed as Protected in the questions and answers section of the listing).

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • o.thornwall
    o.thornwall over 6 years ago in reply to genebren

    Gene, Thanks for the response.

     

    I think you forgot to post the link or address to the batt you are recommending..

     

    And I've see a few vids on fake batts. I agree with you there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to o.thornwall

    Hi Oscar,

    I also agree with Gene, that's the best advice possible, get it from a reputable source, and they will state if the battery is protected or not (either on the web page or the datasheet).

    Often the ones with wires attached will have the protection circuit built-in, but the seller will specify it.

    If you're not buying a battery to fit a holder then for your safety it ought to be a battery with wires attached, not those foil tabs.

    Farnell/Newark has some, and TME.eu has quite a large battery range, and Farnell/Newark and TME.eu are in the group of reputable sellers.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 6 years ago in reply to o.thornwall

    You are so correct.  I guess I have had a little too much exposure to paint fumes today (working on staining my new deck).

     

    Here is the link I was referring too:

     

    https://www.amazon.com/liogea-LG3400G-3400mAh-Rechargeable-Batteries/dp/B07YBTQSQL/ref=sr_1_6?dchild=1&keywords=li-ion+3…

     

    I tend to like batteries that are held in battery holders (replaceable).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • o.thornwall
    o.thornwall over 6 years ago in reply to genebren

    I've already got some LG 18650 3500mAH batts I wish to use, so I'm trying to positively identify the protection device needed to

    attach to my batts. 

    Can anybody advise me on how to go about this ?

     

    I went to the site you suggested.

     

    The batts shown don't come with any "Holders" .

     

    The brands are unknown to me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to o.thornwall

    Hi Oscar,

     

    This is a specialist task done by manufacturers, for building batteries out of raw cells. They don't use a soldering iron for this, they weld the connections onto the cell. Your best bet is returning the cells (if you can), and in any case, buying cells with built-in protection (they come in the form of either either cylinder cells for battery holders, or with insulated wires [and possibly a connector] pre-attached). Some suppliers of such batteries were mentioned earlier.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • o.thornwall
    o.thornwall over 6 years ago in reply to shabaz

    The problem with your idea is I plan on building a  5 cell battery pack later on. But for now I want to start with just one cell. And I will either welding the protection/ BMS to the Batts or soldier them.

     

    Again, my goal is learning how to identify and test the correct protection / BMS PBS for a given application.

     

    Plus making my own cells is substantially cheaper them buying them.

     

    So I have to learn whatever is necessary to make this happen.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • o.thornwall
    o.thornwall over 6 years ago in reply to shabaz

    Sorry but when I responded a minute ago, the technical information you included did not appear.

     

    Where did you find that ? I'd like to investigate that further please.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 6 years ago in reply to o.thornwall

    Hi Oscar,

     

    Do you have a part number on the LG 18650 3500mAH batteries?

     

    Most of the hits I found on "LG 18650 3500mAH" show the battery as 18650 LG INR18650MJ1 3500mAh High Discharge, which is an unprotected cell.  A lot of high discharge batteries are unprotected, to prevent losses at the high current drains.  There are several ICs that will provide protection for the batteries (combinations of over/under voltage and over current).  To find that best IC, you need to understand the conditions that you will normally expect the battery to experience (maximum current draw being the most critical).  If you are not using the battery for it's high discharge capacity (i.e. more for long battery life), the current becomes a little less important.

     

    The important points with Li-Ion batteries:

     

    1. Do not over discharge the batteries.  There are different ways to achieve this.  This can be a part of the battery monitor, or it can be a voltage level detector that can in turn disable the battery discharge path (enable on a regulator, or control to a MOSFET).
    2. Monitor battery temperature during high current discharge.  Do not allow the temperature to exceed the manufacturer's specification (< 75C)
    3. Do not over charge the battery.  The charger or battery management IC can prevent overcharging.

     

    Good luck and be very careful!