Power & Energy
  • Technologies
  • More
Power & Energy
Forum Lipo to Li-Ion Upgrade swap
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 282 subscribers
  • Views 6734 views
  • Users 0 members are here
Related

Lipo to Li-Ion Upgrade swap

o.thornwall
o.thornwall over 6 years ago

Hello All,

The photo attached is of a 3.7v 870mAH Lipo battery. It has a circuit protection PCB (of some kind) attached to it.

 

My goal is to replace this Batt with a Li Ion Batt of the same Voltage but with 3000 mAH of currant.

 

So my question is: Should I remove this protection device and add it to the Li Ion Batt, or should or could I

 

calculate or obtain a new protection device (some how) for the larger mAH battery ?

 

Do I sound like I'm uneducated in the field of electronic ? You'd be right. But I do have some electrical experiencs

 

and I can soldier.

 

Any video explaining this lesson would be greatly appreciated.

 

Thornwall

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +5
    Hi Oscar, Neither : ) You can buy a battery with built-in protection circuit and wires on the end, all pre-assembled reasonably well and partially safe (to a limited extent). The ones without the circuit…
  • o.thornwall
    o.thornwall over 6 years ago in reply to shabaz +2
    1. So Shabaz, your saying the PCB attached to the Batt is a "Protection circuit" device ? 2. How would I discover the exact specification of the "Protection" PCB ? 3. Where would I find a Li-Ion Batt with…
  • genebren
    genebren over 6 years ago in reply to o.thornwall +2
    Thorn, Here is an example of a Li-Ion battery that will meet your specifications. Beware, there are a lot of fake batteries and/or claims out there. Buy from a reputable seller. (Note: these are listed…
Parents
  • shabaz
    shabaz over 6 years ago

    Hi Oscar,

     

    Neither : ) You can buy a battery with built-in protection circuit and wires on the end, all pre-assembled reasonably well and partially safe (to a limited extent).

    The ones without the circuit are intended for specialist use usually (such as to be assembled into a battery pack with specialist equipment).

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • o.thornwall
    o.thornwall over 6 years ago in reply to shabaz

    1. So Shabaz, your saying the PCB attached to the Batt is a "Protection circuit" device ?

     

    2. How would I discover the exact specification of the "Protection"  PCB ?

     

    3. Where would I find a Li-Ion Batt with the maH spec I want, with the correct spec "Protection circuit" PCB ?

     

    I've looked  around alot and havent seen any Li-Ion batts of 3.7v with any "Protection circuit" PCB's attached and for sale ?

     

    Thorn

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 6 years ago in reply to o.thornwall

    Thorn,

     

    Here is an example of a Li-Ion battery that will meet your specifications.  Beware, there are a lot of fake batteries and/or claims out there.  Buy from a reputable seller.  (Note: these are listed as Protected in the questions and answers section of the listing).

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • o.thornwall
    o.thornwall over 6 years ago in reply to genebren

    Gene, Thanks for the response.

     

    I think you forgot to post the link or address to the batt you are recommending..

     

    And I've see a few vids on fake batts. I agree with you there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to o.thornwall

    Hi Oscar,

    I also agree with Gene, that's the best advice possible, get it from a reputable source, and they will state if the battery is protected or not (either on the web page or the datasheet).

    Often the ones with wires attached will have the protection circuit built-in, but the seller will specify it.

    If you're not buying a battery to fit a holder then for your safety it ought to be a battery with wires attached, not those foil tabs.

    Farnell/Newark has some, and TME.eu has quite a large battery range, and Farnell/Newark and TME.eu are in the group of reputable sellers.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 6 years ago in reply to o.thornwall

    Hi Oscar,

    I also agree with Gene, that's the best advice possible, get it from a reputable source, and they will state if the battery is protected or not (either on the web page or the datasheet).

    Often the ones with wires attached will have the protection circuit built-in, but the seller will specify it.

    If you're not buying a battery to fit a holder then for your safety it ought to be a battery with wires attached, not those foil tabs.

    Farnell/Newark has some, and TME.eu has quite a large battery range, and Farnell/Newark and TME.eu are in the group of reputable sellers.