Power & Energy
  • Technologies
  • More
Power & Energy
Forum Lipo to Li-Ion Upgrade swap
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 282 subscribers
  • Views 6785 views
  • Users 0 members are here
Related

Lipo to Li-Ion Upgrade swap

o.thornwall
o.thornwall over 6 years ago

Hello All,

The photo attached is of a 3.7v 870mAH Lipo battery. It has a circuit protection PCB (of some kind) attached to it.

 

My goal is to replace this Batt with a Li Ion Batt of the same Voltage but with 3000 mAH of currant.

 

So my question is: Should I remove this protection device and add it to the Li Ion Batt, or should or could I

 

calculate or obtain a new protection device (some how) for the larger mAH battery ?

 

Do I sound like I'm uneducated in the field of electronic ? You'd be right. But I do have some electrical experiencs

 

and I can soldier.

 

Any video explaining this lesson would be greatly appreciated.

 

Thornwall

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +5
    Hi Oscar, Neither : ) You can buy a battery with built-in protection circuit and wires on the end, all pre-assembled reasonably well and partially safe (to a limited extent). The ones without the circuit…
  • o.thornwall
    o.thornwall over 6 years ago in reply to shabaz +2
    1. So Shabaz, your saying the PCB attached to the Batt is a "Protection circuit" device ? 2. How would I discover the exact specification of the "Protection" PCB ? 3. Where would I find a Li-Ion Batt with…
  • genebren
    genebren over 6 years ago in reply to o.thornwall +2
    Thorn, Here is an example of a Li-Ion battery that will meet your specifications. Beware, there are a lot of fake batteries and/or claims out there. Buy from a reputable seller. (Note: these are listed…
  • genebren
    genebren over 6 years ago in reply to o.thornwall

    Hi Oscar,

     

    Do you have a part number on the LG 18650 3500mAH batteries?

     

    Most of the hits I found on "LG 18650 3500mAH" show the battery as 18650 LG INR18650MJ1 3500mAh High Discharge, which is an unprotected cell.  A lot of high discharge batteries are unprotected, to prevent losses at the high current drains.  There are several ICs that will provide protection for the batteries (combinations of over/under voltage and over current).  To find that best IC, you need to understand the conditions that you will normally expect the battery to experience (maximum current draw being the most critical).  If you are not using the battery for it's high discharge capacity (i.e. more for long battery life), the current becomes a little less important.

     

    The important points with Li-Ion batteries:

     

    1. Do not over discharge the batteries.  There are different ways to achieve this.  This can be a part of the battery monitor, or it can be a voltage level detector that can in turn disable the battery discharge path (enable on a regulator, or control to a MOSFET).
    2. Monitor battery temperature during high current discharge.  Do not allow the temperature to exceed the manufacturer's specification (< 75C)
    3. Do not over charge the battery.  The charger or battery management IC can prevent overcharging.

     

    Good luck and be very careful!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • o.thornwall
    o.thornwall over 6 years ago in reply to genebren

    Hello Gene,

    Does "IC" stand for integrated circuit ?

     

    The Batt I'm looking at has these numbers on it: "LGEBMJ11865 Q218HO62A6" .

     

    Max currant draw under load should be fairly low but I need to rig up a way to test for this under loaded conditions before I can provide this data.

     

    I am using this mAH capacity size for the longer standby time and more run time under load.

     

    I found this info about my choice of batt on the website:

     

     

    Specs (Model: MJ1 in green color):

     

    • Style: Flat Top
    • Chemistry: INR
    • Nominal capacity: 3500mAh
    • Max Continuous Rated Discharge: 10A
    • Dimensions: 65.20 mm (MAX) x 18.50 mm (MAX)
    • Weight: 49.0g (Max)
    • Discharge Cut-off Voltage: 2.5V
    • Nominal voltage: 3.6V~3.7V
    • Full Charge Voltage: 4.2V ± 0.05V
    • Protected: No, Unprotected
    • Standard Charge: CC/CV at 1.70A / 4.20V ± 0.05V
    • Operational Charging Temperature Range: 0 to 45 degrees Celsius
    • Operational Discharging Temperature Range: -20 to 60 degrees Celsius

     

    So these specs are what I have to follow to get the right Charging / protection PCB ?

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 6 years ago in reply to o.thornwall

    Given that you are not using the "High Discharge" aspect of the battery, this device should provide adequate protection (https://www.ebay.com/itm/1S-1A-PCB-Protection-Board-Soler-belt-for-3-7v-18650-Li-ion-lithium-Battery-Cell-/191952871950 )  They seem to have a complete line of devices (some good for up to 15A), so you should be able to find something that will work with your battery.  This is a single cell solution similar to what  shabaz recommended, so this will not address your multiple cell situation.

     

    These devices all seem to have both over and under voltage protection and over current protection.  The selection process, is to find a device that addresses you maximum current draw, under normal conditions, and to provide a safe margin.

     

    Note:  I have no experience with this vendor, so you need to be diligent to insure that you get what you need.

     

    Good luck.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • o.thornwall
    o.thornwall over 6 years ago in reply to genebren

    Hello Gene,

    What exactly does "High Discharge" mean ?

    The link you sent is a great help. You helped putting on the right path. I've been looking for these. But the size and shape is not going to be correct for this application.

    I found a video that shows the round disc protection PCB like shabaz suggested.

     

    But I still need a Battery socket or holder.

    I also need to correctly identify the connector type. If I don't, then I'll have to cut the wires off my old batt, which I prefer not to.

     

    Can you recommend a site that would possibly have a socket or holder and the correct male plug end with wires ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 6 years ago in reply to o.thornwall

    Oscar,

     

    The batteries that you are using can safely be discharged at 10A (which is a very significant about of energy).  This is clearly in the range of 'High Discharge' rate.  I once worked on a medical/cosmetic device that used a single Li-Ion cell to fire a high power laser diode.  We were hitting the laser diode with bursts of 100A pulses.  In order for this to work, we needed and extremely load resistive path in the battery/laser diode path (<5m Ohms), in order to keep the laser diode voltage up high enough to fire.  We were therefor unable to use and in-line form of battery protection.  We relied on monitoring voltage, current and temperature (of both the battery and laser diode), with multiple redundant methods in order to insure that we were safely discharging battery.  In addition, we needed to perform tests, to prove that even in the event of a direct short circuit (with our protection circuits/overrides disabled), that the device would not explode.  It did smoke like crazy and was completely destroyed (case melted and PCB heavily charred), but no explosion.

     

    One interesting thought is to mount the protection circuit on the backside of a battery holder and connect the outputs (protected) of the circuit to your PCB.  There may even be some protection devices from that ebay supplier that are built like that.

     

    Good luck.

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to o.thornwall

    Farnell 2673609 will do you, its a Keystone 1043P, Farnell have no stock at the moment but you

    can get them from Mouser who have > 6000 of them.

    There are other versions with different contacts.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<