Power & Energy
  • Technologies
  • More
Power & Energy
Forum Best way to determine 18650 capacity, resistance and condition ?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 284 subscribers
  • Views 8176 views
  • Users 0 members are here
Related

Best way to determine 18650 capacity, resistance and condition ?

o.thornwall
o.thornwall over 5 years ago

I'd like to get idea on the best way or process to check the capacity, resistance and usable condition of used 18650 batteries ?

I plan on buying several hundreds of these batteries for an up coming project .

 

Thank you, Oscar.

  • Sign in to reply
  • Cancel

Top Replies

  • pctechnocrat
    pctechnocrat over 5 years ago +4
    I have done this for larger battery packs, but the same general method applies for measuring the internal resistance of the cell. Without buying special battery test hardware, you will need an electronic…
  • cookmesomekai
    cookmesomekai over 5 years ago +3
    Reliably determining the state of health of a lithium ion cell is pretty hard to do unless you have a reference cell. If time is not an issue and you have a source, a sink and a power meter available then…
  • jw0752
    jw0752 over 5 years ago in reply to o.thornwall +2
    The problem is defining exactly the point of total discharge, When I test them I fully charge them and then time how long it takes for them to discharge at a specified current to a lower voltage point…
Parents
  • pctechnocrat
    pctechnocrat over 5 years ago

    I have done this for larger battery packs, but the same general method applies for measuring the internal resistance of the cell.  Without buying special battery test hardware, you will need an electronic load and a good quality volt meter, ideally both equipments can be controlled via a computer interface.  Testing the cell at approximately 50% charge (around 3.7V) should yield the most accurate results since this is the most linear region of the charge/discharge voltage curve.  Note ambient temperature of the cell will impact the resistance.

     

    1. Connect the cell using a "4-wire" also called "Kelvin" connection to the programmable load.  This means two wires shorted together at each the positive and negative terminals.  One each of the positive and negative leads will go to the electronic load, the other pair will go to the volt meter.  The purpose of this is to cancel the voltage drop caused by the current through the wire resistance to the load.  Since the volt meter should have very high input resistance (>10Meg Ohms), there is negligible current flowing through the wires to cause a voltage error.

     

    2. Set the load to something like 0.1C current rating of the cell, running in constant current mode.  If your cell is 3000 mA-hr, this would be 300mA current.

     

    3. It is best to automate this measurement sequence, but close enough measurements can be made by manual operation.  The faster the measurements can be made, the less error will be introduced to the measurement since current flowing through the cell will cause self heating (as mentioned, cell temperature will impact the measurement)...generally the thermal mass of the cell and the general low internal resistance will be forgiving if you're not too slow.

     

    4. Start by taking the cell voltage at the 0.1C or 10% current rating of the cell.

     

    5. Step up the load current to something like 0.9C or 90% the current discharge rating of the cell.

     

    6. Take another voltage measurement.

     

    7. Disable the load.

     

    8. Perform some simple math per ohms law to find the resistance:  Voltage = Current * Resistance.  Because this is a linear relationship (for resistive circuits), a delta measurement of current will cause a direct proportional change of the voltage (assuming resistance is constant...which is the assumption we are making).  So then (Voltage_0.1C  - Voltage_0.9C) = (Current_0.9C - Current_0.1C) * Resistance.  Simple algebra yields Resistance = (Voltage_0.1C - Voltage_0.9C) / (Curent_0.9C - Current_0.1C).

     

    For capacity information, you can get decent battery chargers which perform this measurement for roughly $10 per cell slot.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • pctechnocrat
    pctechnocrat over 5 years ago

    I have done this for larger battery packs, but the same general method applies for measuring the internal resistance of the cell.  Without buying special battery test hardware, you will need an electronic load and a good quality volt meter, ideally both equipments can be controlled via a computer interface.  Testing the cell at approximately 50% charge (around 3.7V) should yield the most accurate results since this is the most linear region of the charge/discharge voltage curve.  Note ambient temperature of the cell will impact the resistance.

     

    1. Connect the cell using a "4-wire" also called "Kelvin" connection to the programmable load.  This means two wires shorted together at each the positive and negative terminals.  One each of the positive and negative leads will go to the electronic load, the other pair will go to the volt meter.  The purpose of this is to cancel the voltage drop caused by the current through the wire resistance to the load.  Since the volt meter should have very high input resistance (>10Meg Ohms), there is negligible current flowing through the wires to cause a voltage error.

     

    2. Set the load to something like 0.1C current rating of the cell, running in constant current mode.  If your cell is 3000 mA-hr, this would be 300mA current.

     

    3. It is best to automate this measurement sequence, but close enough measurements can be made by manual operation.  The faster the measurements can be made, the less error will be introduced to the measurement since current flowing through the cell will cause self heating (as mentioned, cell temperature will impact the measurement)...generally the thermal mass of the cell and the general low internal resistance will be forgiving if you're not too slow.

     

    4. Start by taking the cell voltage at the 0.1C or 10% current rating of the cell.

     

    5. Step up the load current to something like 0.9C or 90% the current discharge rating of the cell.

     

    6. Take another voltage measurement.

     

    7. Disable the load.

     

    8. Perform some simple math per ohms law to find the resistance:  Voltage = Current * Resistance.  Because this is a linear relationship (for resistive circuits), a delta measurement of current will cause a direct proportional change of the voltage (assuming resistance is constant...which is the assumption we are making).  So then (Voltage_0.1C  - Voltage_0.9C) = (Current_0.9C - Current_0.1C) * Resistance.  Simple algebra yields Resistance = (Voltage_0.1C - Voltage_0.9C) / (Curent_0.9C - Current_0.1C).

     

    For capacity information, you can get decent battery chargers which perform this measurement for roughly $10 per cell slot.

    • Cancel
    • Vote Up +4 Vote Down