Power & Energy
  • Technologies
  • More
Power & Energy
Forum Can unharnessed electricity/static affect the environment surrounding the source? If so, can it be managed?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 284 subscribers
  • Views 2049 views
  • Users 0 members are here
  • electric mobility
  • static electricity
  • electricty
  • ac voltage
Related

Can unharnessed electricity/static affect the environment surrounding the source? If so, can it be managed?

regannh
regannh over 5 years ago

Hello experts, I'm struggling with an issue that's been difficult and puzzling to address; I hope I've come to the right place for help.

 

I live about 20 yards from an AC/Diesel freight train line (2 tracks and a sizable station a 1/2 mile away.) A main arterial river is 100 yards away, and the immediate environment is a flood zone.

I experience strange things in my apartment, and over nearly a year of confusion and occasionally sheer horror, I believe the signs point to electricity and/or static- ionically charged particles(? not sure of the correct terminology here, forgive my ignorance). It has a visual aspect. If I were to describe it, I'd say it *looks like* current, flowing medium that doesn't fall on the visible light spectrum. But, the light that passes through it is refracted; there is clearly a medium involved.

It appears fluid and affects my textiles in a way that they exhibit a fluid-like movement. Also, many of my things, primarily textiles, appear to off-gas... all. the. time. I witnessed a whitish gas vaporize from a sweatshirt once.

When I try to record the activity with my phone, the video looks very grainy, but I can capture my bedding's legitimate movement, for example.

 

I don't own any measurement devices to verify my guess, and I can't think of anyone, or anywhere I could borrow from.

 

Oddly, I've very rarely been shocked, and it seems only to happen while I'm attempting to eliminate it. Hah!

I've sprayed my entire place - everything, with 50/50 water/fabric softener on 2 occasions, and it doesn't seem to alleviate the activity, although it doesn't worsen it either. I tried a humidifier, albeit before I concluded an ionic charge. The occurrences that followed were terrifying - without getting into detail, specifically, the things that got out of hand involved my several indoor plants.

 

As long as my dog (first) and me (2nd) won't be harmed in the short or long term, I suppose it's okay. It's annoying and kind of creepy, though; it weirds me out, and if possible, I'd prefer to accommodate a tactic to resolve this.

 

Knowledgeable friends out there, do you think my suspicions are likely accurate? Can I measure it, and with what tool/meter? What can I do to address and resolve the issue? Are we facing any risk while living in this environment?

 

Please, and thank you tremendously; any contribution is appreciated.

Regan

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago +5
    Hi Regan, I can not think of any electric field phenomenon that would do what you describe. I have felt the effect of a static electric fields when removing clothes from the clothes dryer in times of low…
  • dougw
    dougw over 5 years ago +4
    Electric trains may run up to 25KV, but for diesel generator trains and some electric trains it is usually 400V to 3000V. I doubt these systems have high electric fields 20 yards away. To measure the field…
  • dougw
    dougw over 5 years ago in reply to regannh +2
    I am not sure which aspect of the video you are referring to, but the fluctuations I see are due to "noise" in the camera sensor. This "optical noise" is due to thermal stimulation in semiconductor junctions…
Parents
  • jw0752
    jw0752 over 5 years ago

    Hi Regan,

     

    I can not think of any electric field phenomenon that would do what you describe. I have felt the effect of a static electric fields when removing clothes from the clothes dryer in times of low humidity and I have seen the effects of a charge field from a Van de Graff generator on the hair of a person that is being charged by it. Electric fields can affect particles in the air as the excess of electrons repel other electrons and attract particles that are deficient in electrons. Static charge is most often induced by friction of one material against another. My sweater rubs against my hair as I take it off or the cat is rubbed with a rubber balloon can produce the effect of a field with excess electrons on one material and an electron deficiency on the other. Sparks will jump from my sweater to my hair and the cat will have a hard time getting rid of the balloon.

     

    Your mention of the nearby railroad makes me think that perhaps there is some low frequency sonic activity that may be shaking dust or things loose but at a frequency that is below the audio level.

     

    A magnetic field would not have an effect on non-ferrous materials such as you describe.

     

    You may want to brush up on your physics and see if you can design a few experiments to get to the bottom of what you describe.

     

    The refractive effects that you describe can be caused by sharp temperature gradients in the air. Sometimes on hot summer days we can see this effect when we look down a black top road that is in the sun and see an almost water like quality to the air.

     

    A good scientist will not rule out anything except magic. I would strongly suspect my own senses before I would accept a supernatural explanation. Get some pictures if possible and get some other skeptical observers involved if possible as this will help better define the phenomena.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 5 years ago

    Hi Regan,

     

    I can not think of any electric field phenomenon that would do what you describe. I have felt the effect of a static electric fields when removing clothes from the clothes dryer in times of low humidity and I have seen the effects of a charge field from a Van de Graff generator on the hair of a person that is being charged by it. Electric fields can affect particles in the air as the excess of electrons repel other electrons and attract particles that are deficient in electrons. Static charge is most often induced by friction of one material against another. My sweater rubs against my hair as I take it off or the cat is rubbed with a rubber balloon can produce the effect of a field with excess electrons on one material and an electron deficiency on the other. Sparks will jump from my sweater to my hair and the cat will have a hard time getting rid of the balloon.

     

    Your mention of the nearby railroad makes me think that perhaps there is some low frequency sonic activity that may be shaking dust or things loose but at a frequency that is below the audio level.

     

    A magnetic field would not have an effect on non-ferrous materials such as you describe.

     

    You may want to brush up on your physics and see if you can design a few experiments to get to the bottom of what you describe.

     

    The refractive effects that you describe can be caused by sharp temperature gradients in the air. Sometimes on hot summer days we can see this effect when we look down a black top road that is in the sun and see an almost water like quality to the air.

     

    A good scientist will not rule out anything except magic. I would strongly suspect my own senses before I would accept a supernatural explanation. Get some pictures if possible and get some other skeptical observers involved if possible as this will help better define the phenomena.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Children
  • regannh
    regannh over 5 years ago in reply to jw0752

    Thank you, John, So much! This is very helpful, and rules out this idea. I'm perfectly okay with process of elimination. I absolutely agree with you - no magic, and I've personally dismissed the idea of the supernatural also.

     

    Other rabbit holes I've considered are VOC's, with this being a newly renovated building - laminate flooring, drywall, adhesives, etc. Also, I thought maybe there's actually an organism, like a fungus in its early life stage (the building the 110 years old and for the majority of its lifetime served as grain storage.)  Electrokinetic phenomena sounded logical and reasonable, considering this prous concrete building in an area that meets water annually.

    I don't have a college education in any of the fields around what I've brought up so I can't say I have much to go off of with these ideas. With hindsight being 2020, I certainly would have Loved, and wish I would've taken a science route in college.

     

    I completely understand this sounds off the deep end... and I truly have questioned my eyesight, optic nerve, and yes, mental statusas well. I'm a realist, I'm extremely self-aware, and I put all my eggs in science, logic and rationale.

    It's difficult to even initiate these discussions; I'm flabbergasted and frankly, embarrassed to attempt them. I 100% guarantee this will be the last time it leaves my brain image  It's especially hard when I can collect a measurable result in what's happening - make a mark where it was at first notice, then make a mark after "movement." There's a space. Or, a sizable amount of width if it was a pillow that puffed up with no apparent reason. Anyway, I digress.

     

    I can go through some of my videos I've collected and add them here if you're curious, but I'm not sure what further would come of it. I like your idea of keeping on with the experiments and check off what it isn't. Maybe I should just move! image

     

    Thank you again for your response - I genuinely appreciate your respectful insight!