Power & Energy
  • Technologies
  • More
Power & Energy
Forum 18650 Battery Length Variation
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 281 subscribers
  • Views 8712 views
  • Users 0 members are here
  • lithium-ion_battery
  • 18650 cell
  • battery_protection
Related

18650 Battery Length Variation

ralphjy
ralphjy over 5 years ago

I just committed an inadvertent blunder that I thought I'd share in case it might help others.

 

I ordered a couple of 18650 Lithium Ion batteries for a robot vehicle that I'm building.  I saw that these batteries were "protected" at the point that I ordered them, but did not consider the implication - after all an 18650 has a standard dimension as the name suggests, right?  Well, it turns out that the protection circuit increases the length of the battery - in this instance by slightly more than 3 mm and I'd probably have to destroy the battery holder to get them to fit.  Oh well, I can probably use these in a flashlight image.  I'll need to order new unprotected ones for the robot.  I'm a little surprised that the clips in the battery holder don't give a little more.

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 5 years ago +4
    Most Li-Ion batteries come in several types - - Large Button - these cells have large and wide contact areas which protrude from the positive side of the cell, usually only by a small amount. This allows…
  • genebren
    genebren over 5 years ago +2
    Ralph, Protected refers to preventing reverse insertion of the battery (at least for a button top battery). Protected holders have a rim constructed around the positive contact such that only the button…
  • ralphjy
    ralphjy over 5 years ago in reply to javagoza +2
    Obviously, I didn't do a good job of checking the specs either ... It was a combo kit of two batteries and a charger from Dantona Industries (China) that I bought on DigiKey https://www.digikey.com/en…
Parents
  • genebren
    genebren over 5 years ago

    Ralph,

     

    Protected refers to preventing reverse insertion of the battery (at least for a button top battery).  Protected holders have a rim constructed around the positive contact such that only the button top fits into the opening. You can not reverse the insertion.  I have had some luck in clipping out the rim around the contact and using it with a non-button top battery.

     

    Good luck!
    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 5 years ago

    Ralph,

     

    Protected refers to preventing reverse insertion of the battery (at least for a button top battery).  Protected holders have a rim constructed around the positive contact such that only the button top fits into the opening. You can not reverse the insertion.  I have had some luck in clipping out the rim around the contact and using it with a non-button top battery.

     

    Good luck!
    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ralphjy
    ralphjy over 5 years ago in reply to genebren

    Gene,

     

    This is actually a protected battery not a protected holder.  Unfortunately, it would not prevent the battery from making contact if it were inserted backwards.  I’m thinking that this holder is designed for flat top batteries, but I probably could have used a button top without the extra length - I could be wrong.  I’ve ordered flat tops that have the length dimension specified.

     

    Ralph