Power & Energy
  • Technologies
  • More
Power & Energy
Forum Why PWM generate circuit can not adjust the duty cycle to 10%?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 286 subscribers
  • Views 2001 views
  • Users 0 members are here
  • duty
  • pwm
  • led
  • cycle
  • dimming
Related

Why PWM generate circuit can not adjust the duty cycle to 10%?

Jason
Jason over 15 years ago

I have a problem when I am debuging. My PWM generate circuit can not adjust the duty cycle to 10%! It just 46% when I modulate Rp_Potentiometer.SCH.jpg

 

But I have checked the circuit by a software called EWB and the follow images are test result.

 

1 R_potentiometer =100k Ohm  100%

   Duty cycle=10%

image

 

2 R_potentiometer =100k Ohm   50%

   Duty cycle=50%

image

 

3 R_potentiometer =100k Ohm      0%

   Duty cycle=90%

image

 

Why? Can anyone tell me why!

  • Sign in to reply
  • Cancel
Parents
  • WarrenW
    WarrenW over 15 years ago

    You could always try using a PICAXE 08M micro to generate your PWM. These are good for 0% - 100% and are adjustable by simple basic programing.

    image

    Effectively you would put your pot between 0V and +V with the wiper connected to Pin 6 (ADC 1) and use Pin 5 (PWM2) to generate your pulses, this can be isolated via a mosfet if more drive is required. Apart from a 5V regulated supply thats all you need!

     

    Program the micro with the code along the lines of....

     

    ;INPUT PIN 6 (ADC1)
    ;OUTPUT PIN 5 (PWM2)

    SYMBOL ADCVALUE = W1  ;ASSIGN WORD 1

    MAIN:
    READADC10 1,ADCVALUE  ;Reads the Voltage off the pot and assigns a number 0-1024
    PWMOUT 2,150,ADCVALUE  ;The PWM period (150 IN THIS CASE) = (period + 1) x 4 x resonator speed (1/4000000) effectively = the number + 1 in uS
    GOTO MAIN

    ;THE DUTY CYCLE IS DETERMINED BY THE 'ADCVALUE FIGURE' 0 = 0% AND 1024 = 100%
    ;SCALING CAN BE DONE VIA CALCULATION WITHIN THE PROGRAM
    ;E.G LABEL PWMVAL =W2
    ;AFTER READING THE ADCVALUE IT CAN BE MANIPULATED
    ;LET PWMVAL = ADCVALUE/2 (EFFECTIVELY A 0-50% PWM)

     

     

    Picaxe chips, software (free) etc can be obtained from www.picaxe.co.uk

     

    Cheers

    Warren.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • WarrenW
    WarrenW over 15 years ago

    You could always try using a PICAXE 08M micro to generate your PWM. These are good for 0% - 100% and are adjustable by simple basic programing.

    image

    Effectively you would put your pot between 0V and +V with the wiper connected to Pin 6 (ADC 1) and use Pin 5 (PWM2) to generate your pulses, this can be isolated via a mosfet if more drive is required. Apart from a 5V regulated supply thats all you need!

     

    Program the micro with the code along the lines of....

     

    ;INPUT PIN 6 (ADC1)
    ;OUTPUT PIN 5 (PWM2)

    SYMBOL ADCVALUE = W1  ;ASSIGN WORD 1

    MAIN:
    READADC10 1,ADCVALUE  ;Reads the Voltage off the pot and assigns a number 0-1024
    PWMOUT 2,150,ADCVALUE  ;The PWM period (150 IN THIS CASE) = (period + 1) x 4 x resonator speed (1/4000000) effectively = the number + 1 in uS
    GOTO MAIN

    ;THE DUTY CYCLE IS DETERMINED BY THE 'ADCVALUE FIGURE' 0 = 0% AND 1024 = 100%
    ;SCALING CAN BE DONE VIA CALCULATION WITHIN THE PROGRAM
    ;E.G LABEL PWMVAL =W2
    ;AFTER READING THE ADCVALUE IT CAN BE MANIPULATED
    ;LET PWMVAL = ADCVALUE/2 (EFFECTIVELY A 0-50% PWM)

     

     

    Picaxe chips, software (free) etc can be obtained from www.picaxe.co.uk

     

    Cheers

    Warren.