Power & Energy
  • Technologies
  • More
Power & Energy
Forum Free energy?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 288 subscribers
  • Views 4179 views
  • Users 0 members are here
Related

Free energy?

enrico.migchels
enrico.migchels over 16 years ago

Hi there,

 

There are several posts on the Internet from people who claim to have found the energy 'holy grail'. Meaning machines which convert energy from one form the another without loss or even with energy gain. What do we do which such claims as there is no one who has produced a machine that is in normal use somewhere by someone.

 

Personally i am strong non-believer of free energy devices, as they seem to contradict the law's of physicsas as we know them.

 

Please share your idea's and comments on this topic.

 

Best regards,

 

Enrico Migchels

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 14 years ago in reply to FredM +2
    Personally, I find that sanity is just social concensus. 6443.contentimage_938.png I am amazed at the number of people that think we have an energy shortage. From my analysis, we are using just a small…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi, -This is my first topic so I hope I won't make mistake. I strongly agree with you, but sometime it's possible to "harvest" a small quantity of energy that can be used to produce energy. For example…
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor +1
    Hey, new to this, but very interested in converting heat to electricity! Can you explain the theory behind a pelcier cell? I'm having a little trouble finding anyone to explain it to me, it seems like…
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi,

    -This is my first topic so I hope I won't make mistake.

     

    I strongly agree with you, but sometime it's possible to "harvest" a small quantity of energy that can be used to produce energy. For example it is possible (and it's quite simple) to use a Peltier cell to convert heat into electricity. Some years ago I've built a very simple circuit that can power a LED with a small Peltier cell (40x40) and the heat of my body. Now I'm looking on Tesla generator that sems to be able to harvest energy field and produce a very small quantity of energy (mW) that could be use with sensor network.

     

    I've read something about Bruce De Palma but I think it N-machine ca not work.

     

    The REAL WAY TO "PRODUCE" ENERGY IS TO REDUCE THE WASTE OF ENERGY or TO CONVERT "USELESS" ENERGY (Heat, wind, sun, electomagnetic fields).

     

    Hi!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hey, new to this, but very interested in converting heat to electricity!

    Can you explain the theory behind a pelcier cell? I'm having a little trouble finding anyone to explain it to me, it seems like an amazing technology though that could possibly revolutionize technology!

     

    Thanks ahead of time 3660.contentimage_1.png

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    I'm not sure I can be clear. It's about the kinematic energy due at thermal energy. More is the thermal energy and more is the kinematic energy that all the electrons have. If, in a diode (the peltie cell is like a big diode), an electron has sufficent energy can "jump" the potential barrier becomes "free" and can be used.
    Appropriately doping and sizing the junction you can have sufficent electrons and the potential barrier.
    I hope it clear... but ask for any question!
    Hi!

    I'm not sure I can be clear. It's about the kinematic energy due at thermal energy. More is the thermal energy and more is the kinematic energy that all the electrons have. If, in a diode (the peltie cell is like a big diode), an electron has sufficent energy can "jump" the potential barrier becomes "free" and can be used.

    Appropriately doping and sizing the junction you can have sufficent electrons and the potential barrier.

    I hope it clear... but ask for any question!

    Hi!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • awinning
    awinning over 15 years ago in reply to e14 Contributor

    I've talked to a few of our suppliers recently and energy harvesting is a big topic for them. Linear Technology, TI and Microchip all have solutions to collect and store energy from natural phenomenom like heat, light and vibration. The circuits consist of a collector such as a solar panel, conversion and a storage battery. Sometimes the circuits have a supplemental battery.

     

    The suppliers are claiming that these circuits can power an sensor, MCU and a Zigbee type measurement node for ten years and upwards.

     

    But I think you may be referring to cold fusion type circuits, which many invertors claim to have made. All these claims have proved impossible to replicate under controlled conditions. It is a fascinating subject and I watched a great show on it once

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • enrico.migchels
    enrico.migchels over 15 years ago in reply to awinning

    Hi,

     

    Energy harvesting is indeed interesting and well understood. Look for example to solar energy. The sun produces around 1300W/m^2 of which 1000W/m^2 reaches the ground. We are able to convert 20% of the energy to electricity with the best PV-cells available. That's 200W!. The backdraw of this is the technology behind the conversion. Traditionally you would need a solar charger and battery storage device and inverter to make use of the energy. Lot's of converters, lot's of losses, lot's of money spent. The modern way of converting the solar energy is to pump it directly (via 1 boost/inverter stage) into the grid. You need the support of your electricity company to do this. For stand-alone application solar energy is nice, could even be cheaper than connecting to the grid (if the grid is not there yet) but you have to oversize the solar panel enormous to have sufficient energy the whole year round. As the winter time is really a problem for the energy harvesting (energy output may reduce to 10% of the nominal value) the system becomes relative expensive. I would say: focus on the application and make a overall efficient system. Most energy is wasted in the application. I thing is clear: if you build a solar application you MUST consider all aspects of the system and finetune each component for optimal performance. If not, your customer is disappointed. There are a lot of those around as several solar products have very poor performance. Engineers have to be educated about the do's and don't of solar technology. If not the general public will turn there back on solar products. Or: who want a solar energy driven flashlight? :-)

     

    Best regards, Enrico Migchels

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • M0DCD
    M0DCD over 15 years ago in reply to enrico.migchels

    In applications I have used solar, it's been that they are either off the grid or just require power intermittantly. Then it's usually the storage device that limits its use. One problem is that at higher latitudes, the use may be more when the nights are longer, and the weather worse, so you can end up with having to over specify the solar input side to get the required energy into the system. Solar powered lighting for the Developing World is a real application, as it reduces their reliance on such as kerosene for lighting and has obvious safety advantages.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    For some applications (military) It is possible to use the seeback effect to produce energy that can be used for sensors. The thermal energy comes from the sun: the sensor is inside a rock (black?) which surfice become hot thanks to the solar energy. The thermal difference between the rock and the ground give enough energy to power the sensor.
    Where I work there are some different sistem: 3 geothermal sistems and 3 solar sistems (2 therma solar system and 1 photvoltaic system). The photovoltaic sistem it's about 19kWp and we sell the energy to the main company. Due to energy lost, we sell about 0,93 of the total energy that solar pannels can produce.
    It's very interesting to see what happen when rein or there are some clouds... the drop of power it's impressive.
    I hope think film pannel can allow to reduce the cost of the system that is too hight.
    I've founded some information about something called "Tesla's Antenna" that can convert "static energy" into electricity that can be used to power sensors. Someone has been tryed to build a Tesla generator?For some applications (military) It is possible to use the seeback effect to produce energy that can be used for sensors. The thermal energy comes from the sun: the sensor is inside a rock (black?) which surfice become hot thanks to the solar energy. The thermal difference between the rock and the ground give enough energy to power the sensor.
    Where I work there are some different sistem: 3 geothermal sistems and 3 solar sistems (2 therma solar system and 1 photvoltaic system). The photovoltaic sistem it's about 19kWp and we sell the energy to the main company. Due to energy lost, we sell about 0,93 of the total energy that solar pannels can produce.
    It's very interesting to see what happen when rein or there are some clouds... the drop of power it's impressive.
    I hope think film pannel can allow to reduce the cost of the system that is too hight.
    I've founded some information about something called "Tesla's Antenna" that can convert "static energy" into electricity that can be used to power sensors. Someone has been tryed to build a Tesla generator?
    For some applications (military) It is possible to use the seeback effect to produce energy that can be used for sensors. The thermal energy comes from the sun: the sensor is inside a rock (black?) which surfice become hot thanks to the solar energy. The thermal difference between the rock and the ground give enough energy to power the sensor.
    Where I work there are some different sistem: 3 geothermal sistems and 3 solar sistems (2 therma solar system and 1 photvoltaic system). The photovoltaic sistem it's about 19kWp and we sell the energy to the main company. Due to energy lost, we sell about 0,93 of the total energy that solar pannels can produce.
    It's very interesting to see what happen when rein or there are some clouds... the drop of power it's impressive.
    I hope think film pannel can allow to reduce the cost of the system that is too hight.
    I've founded some information about something called "Tesla's Antenna" that can convert "static energy" into electricity that can be used to power sensors. Someone has been tryed to build a Tesla generator?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    don't need, ask the goverment for ur solar panel support, then pay some

    for yourself, few years later, you get true free energy.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    With this kind of "application" it's very important the "insurance": inverters are very fragile and after few years can broken. If you have some problems and you have to change some pannels you may not be able to install the same kind (ame voltage and current) of pannel: so the performance of you system can become very low due to the "incompatibility" of the new pannels. For example: you have a system of 7 pannels and if, after 10 years, you have to change a pannel moving from In=10A to In=5A, all the system can erogate 5A at maximum...
    If you have to change the inverter you have to wait for the new one: In "my" system I had to wait for a month... so the system was down for a month and it was not able to produce energy and money.
    I call that "TRUE LIFE"...
    And, as last... WE pay the goverment: so WE pay for solar energy... I'm not sure we can call the Solar energy as "free energy".
    I think that solar energy it's usefull only with small and distribuite applications.

    With this kind of "application" it's very important the "insurance": inverters are very fragile and after few years can broken. If you have some problems and you have to change some pannels you may not be able to install the same kind (ame voltage and current) of pannel: so the performance of you system can become very low due to the "incompatibility" of the new pannels. For example: you have a system of 7 pannels and if, after 10 years, you have to change a pannel moving from In=10A to In=5A, all the system can erogate 5A at maximum...

    If you have to change the inverter you have to wait for the new one: In "my" system I had to wait for a month... so the system was down for a month and it was not able to produce energy and money.

     

    I call that "TRUE LIFE"...

     

    And, as last... WE pay the goverment: so WE pay for solar energy... I'm not sure we can call the Solar energy as "free energy".

     

    I think that solar energy it's usefull only with small and distribuite applications.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    I find the EuroDish stirling generators quite interesting, as they use a parabolic mirror to concentrate light onto a small chamber which inturn heats water that drives a stirling engine, however this system also has flaws mainly in cost and maintainence. I think it would be neat if we could convert existing fossil fuel plants, which burn fuels to generate steam and so drive turbines, to instead generate steam using geothermal energy of the earth. As far as free energy goes (as in free for me) I have used static generators before to power small sensors with moderatly good results, luckly I'm near a TV transmission tower.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>