Power & Energy
  • Technologies
  • More
Power & Energy
Forum No plugs, slot based power strips
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 284 subscribers
  • Views 400 views
  • Users 0 members are here
  • dc-dc
  • management
  • power_management
  • power_distribution
  • power_strip
  • Design
  • power_supply
  • power_conversion
  • power
  • power.power
Related

No plugs, slot based power strips

Catwell
Catwell over 15 years ago
As I was frantically trying to wedge the plug of my cell phone into a power strip that was dangerously full, I thought of this concept I saw recently. I can't believe this hasn't been made already.
 
image

Often enough concepts never make it too the market, I hope that this one will. Or at least a knock off. I think the NEMA 5–15 (North American 15 A/125 V grounded) three prong plug would be easier to make a strip for than the Type I, 3 prong, shown above.

I would like to see this made in a similar way, but with a really heavy base. I hate when power strips flip or fall over.

Cabe
  • Sign in to reply
  • Cancel
Parents
  • enrico.migchels
    enrico.migchels over 15 years ago

    Hi Cabe,

     

    I trust that the there are multiple spring fingers in the device making sure that the contact pressure is always good, regardless where a plug is positioned? Such a device will never hit the market in Europe as it is too easy for infants to put small (metal) parts in with serious consequences. In Europe new sockets have a plastic shield which is pressed aside when a plug is inserted. Anyway, the idea is certainly interesting.

     

    Best regards, Enrico Migchels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Catwell
    Catwell over 15 years ago in reply to enrico.migchels

    Enrico,

     

    I was thinking the exact same thing. However, I think these would be an absolute must for labs, work stations, and the like.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Catwell
    Catwell over 15 years ago in reply to enrico.migchels

    Enrico,

     

    I was thinking the exact same thing. However, I think these would be an absolute must for labs, work stations, and the like.

     

    Cabe