Power & Energy
  • Technologies
  • More
Power & Energy
Forum Fusion reactor to create mini sun on earth
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 284 subscribers
  • Views 3024 views
  • Users 0 members are here
  • alternative_energy
  • alternative
  • reactor
  • fusion
  • energy_harvesting
  • energy
  • solutions
Related

Fusion reactor to create mini sun on earth

Eavesdropper
Eavesdropper over 15 years ago
image
Scientists at the National Ignition Facility in Livermore California hope to have the world’s first sustainable fusion reactor powered up and running by 2012. Guessing by the ancient Mayan calendar that say’s the world will end by that year, scientists speculate the sun will no longer function and need a ‘replacement’ to missile off to the center of the solar system. Seriously though, engineers designed the reactor to use 192 lasers aimed at small BB sized glass targets that house the hydrogen isotopes tritium and deuterium. The lasers simultaneously, in a fraction of a second, pulsate ultraviolet laser energy (equivalent to two million joules) to their respective targets. The resulting energy released through this process, known as inertial confinement fusion, was around 1.3 million mega joules which created a peak core temperature of six million degrees Farenheight, about the same amount of energy and heat found in a small star or large planet. This is the first laser in which the energy released is greater than the energy used to make the fusion reaction. (I am dubious.) The NIF hope to replace existing nuclear power plants with a more safe and refined fusion plant that could theoretically handle a quarter of the United States energy consumption by 2050. Let’s just hope these fusion plants don’t go nova on us. For a more detailed abstract view and process explanationg visit NIF’s website at: https://lasers.llnl.gov/
 
Eavesdropper
  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 15 years ago

    I have watched this technology evolve over the last forty years and while I like the promise of the process, I am still a little concerned over their ability to contain the reaction once they initiate it.  The sun has the huge mass in which to contain the fusion energy.  I am not sure if these scientist have considered the full consequence of a full fusion reaction under these conditions.

    I suspect there are still issues about Fusion that we do not fully understand.  So the claim that this approach will be cleaner than fission is not fully validated to my satisfaction.

    Thanks,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 15 years ago

    I have watched this technology evolve over the last forty years and while I like the promise of the process, I am still a little concerned over their ability to contain the reaction once they initiate it.  The sun has the huge mass in which to contain the fusion energy.  I am not sure if these scientist have considered the full consequence of a full fusion reaction under these conditions.

    I suspect there are still issues about Fusion that we do not fully understand.  So the claim that this approach will be cleaner than fission is not fully validated to my satisfaction.

    Thanks,

    DAB