Power & Energy
  • Technologies
  • More
Power & Energy
Forum Fusion reactor to create mini sun on earth
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 283 subscribers
  • Views 3095 views
  • Users 0 members are here
  • alternative_energy
  • alternative
  • reactor
  • fusion
  • energy_harvesting
  • energy
  • solutions
Related

Fusion reactor to create mini sun on earth

Eavesdropper
Eavesdropper over 15 years ago
image
Scientists at the National Ignition Facility in Livermore California hope to have the world’s first sustainable fusion reactor powered up and running by 2012. Guessing by the ancient Mayan calendar that say’s the world will end by that year, scientists speculate the sun will no longer function and need a ‘replacement’ to missile off to the center of the solar system. Seriously though, engineers designed the reactor to use 192 lasers aimed at small BB sized glass targets that house the hydrogen isotopes tritium and deuterium. The lasers simultaneously, in a fraction of a second, pulsate ultraviolet laser energy (equivalent to two million joules) to their respective targets. The resulting energy released through this process, known as inertial confinement fusion, was around 1.3 million mega joules which created a peak core temperature of six million degrees Farenheight, about the same amount of energy and heat found in a small star or large planet. This is the first laser in which the energy released is greater than the energy used to make the fusion reaction. (I am dubious.) The NIF hope to replace existing nuclear power plants with a more safe and refined fusion plant that could theoretically handle a quarter of the United States energy consumption by 2050. Let’s just hope these fusion plants don’t go nova on us. For a more detailed abstract view and process explanationg visit NIF’s website at: https://lasers.llnl.gov/
 
Eavesdropper
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    I find this whole idea totally  assinine.  Why would anyone even surmize to venture into such as is this realm. Man is not capable of duplication of the sun, period. Nor is he at all capable of the dealing with the consequence should he even minutely devise even a hint of so doing. As per the nuclear energy of today, it is for sure a real joke. To take pot shots at glass BBS is for real incomprehensionable. Heat, but for sure, lets just dump a bunch of water on it, maybe it will all go away, that we may expend our future time on even more nonesense. Such thinking as this is indeed pure folic....Man needs to find an upright means of deserting his cubicle, and sorta see what life is really all about. Sure, to produce the energy of the sun is not at all a problem, but, to create a sun itself, well man may want to coverse with his own creator first, lest he venture beyound the given realm of his own destiny, and not find his way back.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    I find this whole idea totally  assinine.  Why would anyone even surmize to venture into such as is this realm. Man is not capable of duplication of the sun, period. Nor is he at all capable of the dealing with the consequence should he even minutely devise even a hint of so doing. As per the nuclear energy of today, it is for sure a real joke. To take pot shots at glass BBS is for real incomprehensionable. Heat, but for sure, lets just dump a bunch of water on it, maybe it will all go away, that we may expend our future time on even more nonesense. Such thinking as this is indeed pure folic....Man needs to find an upright means of deserting his cubicle, and sorta see what life is really all about. Sure, to produce the energy of the sun is not at all a problem, but, to create a sun itself, well man may want to coverse with his own creator first, lest he venture beyound the given realm of his own destiny, and not find his way back.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Man is capable of creating a "SUN" We call them Thermonuclear (Hydrogen) bombs and there are many thousands of them. They're small and short lived but do the job that was intended of them

     

    Jeff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    I would assume that the seawater is simply being used as a source of deuterium.

     

    Only one part in 6500 is deuterium and it's uneconomical to attempt to extract more than a small fraction of it. What's left is 99.995% of the original water which is perfectly safe to dump back where it came from, although a fair proportion of it will have been sufficiently purified en route to be saleable as a product in itself (or used on-site). You'd probably use ten gallons of "liquid deuterium ore", not just one, to pull out a few grams of deuterium oxide - the equivalent of 300 gallons of gasolene.

     

    That would be in a reactor which, mark you, doesn't yet exist. Getting fusion fuel never was a problem, creating a reactor most definitely is.