Power & Energy
  • Technologies
  • More
Power & Energy
Forum Programmable timer to drive 230V siren for sports ground
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 283 subscribers
  • Views 781 views
  • Users 0 members are here
Related

Programmable timer to drive 230V siren for sports ground

e14 Contributor
e14 Contributor over 13 years ago

Hi, I'm new to Arduino and am impressed with the vast array of projects that turn up! I want to make a programmable timer to drive a siren periodically. Basically I want it to drive the siren for a 6 sec blast at set times throughout the day. I have hunted around for a similar project as I'm sure it's been done but am not having any luck. Does anyone know of one that will suit my purpose? Any assistance in being shown where to start would be most appreciated.

 

cheers,

Andy

  • Sign in to reply
  • Cancel
Parents
  • fidelsalinas
    fidelsalinas over 13 years ago

    I'd use a relay and set one of your pins to 5v output on a 6 second loop during the chosen time periods. It's almost the same as the blinking LED

     

    int outPin = 13;


    void setup()

    {

         pinMode(outPin, OUTPUT);

    }


    void loop()

    {

         digitalWrite(outPin, HIGH);

         delay(60000);

         digitalWrite(outPin, LOW);

         delay(time to next trigger);

    }

    connect pin 13 and ground of your arduino to the triggering side of the relay, Then connent the sirens Positive lead to the other two inputs on the relay and ground to it's ground. when your arduino sets the 5v output it acts as a switch conneting the positive line, giving your siren power.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to fidelsalinas

    Thanks Fidel,

     

    As I understand it there are three components to this project:

    1. A clock set with the correct date/time
    2. Ability to program times to drive the relay (eg, 8:50am, 9am, 9:20am, 9:30am, 9:50am etc)
    3. The relay

     

    I'm a real newbie starting form the ground up here...

     

    cheers,

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fidelsalinas
    fidelsalinas over 13 years ago in reply to e14 Contributor

    yup, thats pretty much the drift of it, adding a real time clock would help for exact times and dates. I hope you get your project up and running and if you run into problems i'm more then happy to help.

     

    regards,

    Fidel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fidelsalinas
    fidelsalinas over 13 years ago in reply to e14 Contributor

    yup, thats pretty much the drift of it, adding a real time clock would help for exact times and dates. I hope you get your project up and running and if you run into problems i'm more then happy to help.

     

    regards,

    Fidel