Power & Energy
  • Technologies
  • More
Power & Energy
Forum circuit for our requirement
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 283 subscribers
  • Views 392 views
  • Users 0 members are here
Related

circuit for our requirement

e14 Contributor
e14 Contributor over 12 years ago

dear sir , in my project the control voltage is 0 to 5 V and this control voltage use we varies the the heater which is 230 v operate.suppose output control voltage is 5 volt then heater operate 230 v if control voltage is less then 5 then heater works less then operate 230 v. using these we temperature controlling of tank . so , kindly help me for this types of circuit design....

 

 

 

 

 

 

thanks..

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    what is the power/current level of the heater?

    is this a pure resistive load? or you would need also a PFC on top?

    you can achieve this in 2 ways: with a voltage regulator (more difficult, since you should act on 230AC in directly) or by using an AC LED driver (you use the 5V command to change the output current, as a dimming signal basically)...

    please have a look at the product page

    http://www.ti.com/lit/ds/symlink/tps92410.pdf

    KR

    Vincenzo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Unfortunately I'm not sure either of these are suitable. A solid state relay (SSR) will work, provided you have a circuit to transform your control voltage (0-5V) into a pulse width modulated train. But, if the poster is asking this question, I'm not sure it is safe to be experimenting with mains powered heaters anyway.