Power & Energy
  • Technologies
  • More
Power & Energy
Forum Multiple output DC to DC converter
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 284 subscribers
  • Views 618 views
  • Users 0 members are here
  • l293d
  • h-bridge
  • arduino
  • dc-to-dc
Related

Multiple output DC to DC converter

e14 Contributor
e14 Contributor over 11 years ago

Hi everybody.

 

I am working on a Arduino project using H-bridge (L293D) to drive two motors and I would like to have my project to be powered by an unique power source.

I have an AC/DC power supply that is outputting ~16V at ~1000mA and I am wondering if it is possible to get a stable +5V for the Arduino and the remaining for the motors via the H-Bridge

 

Is It possible and how to achieve that ? voltage divider (going down from 16V to 5V seems a waste) ?

 

Thx in advance for any help you can bring

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    why not go to simpler solutions rather than making it so complex.

    Connect the two in parallel series and apply resistors to reduce the voltage to required levels if voltage is to be reduced and current is not of concern.

    But if current is to be kept the same the connect them in series and then apply resistors as required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago

    Hi Cedric,

    I would use a 7805 voltage regulator IC to drop the power down to 5 volts for the Arduino. While you are correct that the drop from 16 to 5 volts will require that some energy be dissipated by the regulator it should be no problem as the power handling of a 7805 will exceed the output power of your AC Adapter. The Arduino will use different amounts of current depending on the coding and the circuits that you are driving with its output pins. A 100mA draw from the Arduino would require the 7805 to dissipate 1.1 Watts. It would probably be best if you heat sink the 7805. Keep an eye on your over all power consumption as your power supply with 16 volts and 1000 mA has about 16 Watts that it can supply. Your motors and H bridge circuitry will have to be factored in.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 11 years ago

    I would provide separate supplies for the logics and for the drives, and use an opto-isolator to facilitate communication between them.  The requirements for the two supplies are divergent.  It is churlishly cheap to try to get a twofer here.