Power & Energy
  • Technologies
  • More
Power & Energy
Forum Multiple output DC to DC converter
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 284 subscribers
  • Views 620 views
  • Users 0 members are here
  • l293d
  • h-bridge
  • arduino
  • dc-to-dc
Related

Multiple output DC to DC converter

e14 Contributor
e14 Contributor over 11 years ago

Hi everybody.

 

I am working on a Arduino project using H-bridge (L293D) to drive two motors and I would like to have my project to be powered by an unique power source.

I have an AC/DC power supply that is outputting ~16V at ~1000mA and I am wondering if it is possible to get a stable +5V for the Arduino and the remaining for the motors via the H-Bridge

 

Is It possible and how to achieve that ? voltage divider (going down from 16V to 5V seems a waste) ?

 

Thx in advance for any help you can bring

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    D_Hersey over 11 years ago

    I would provide separate supplies for the logics and for the drives, and use an opto-isolator to facilitate communication between them.  The requirements for the two supplies are divergent.  It is churlishly cheap to try to get a twofer here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • D_Hersey
    D_Hersey over 11 years ago

    I would provide separate supplies for the logics and for the drives, and use an opto-isolator to facilitate communication between them.  The requirements for the two supplies are divergent.  It is churlishly cheap to try to get a twofer here.