Power & Energy
  • Technologies
  • More
Power & Energy
Forum Isolated DC-DC converters in series
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 282 subscribers
  • Views 1792 views
  • Users 0 members are here
  • series
  • dc_dc_converter
Related

Isolated DC-DC converters in series

sunnyiut
sunnyiut over 10 years ago

Hello everyone,

I am using two wireless charging modules for powering my circuit. The receiver part has 5v DC DC buck converter and I would like to connect the output of two modules in series to form a +/- 5v dual supply.

imageimage

 

Is there any chance of damaging any of the converters if I directly connect these in series? I have found that VicroPower and SynQor suggest to use protection diode at the output. These diodes are for preventing back-feeding by load capacitance during turn-off, and assuring proper operation during start-up and dynamic loading. Also prevent the output from going negative if only one converter is operational [like in case of thermal shutdown of one converter].

high voltage outputimage

Now, as my DC DC converters are totally isolated at the input side [two separate coils], do I need to use those protection diodes?

  • Sign in to reply
  • Cancel
  • peterjcs23
    0 peterjcs23 over 10 years ago

    The vicor scheme looks different as it is a 0 to 10V output, where as you are proposing a +5..0..-5V scheme. The vicor scheme could end up with one output feeding through the other but your scheme will not do that. No need for diodes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago

    I would use the diodes, if you use schottky diodes there won't be too much voltage drop. The reason is that if you have a reasonable capacitance in the load and one supply drops out for any reason then the other can get double the single supply voltage applied to its output, which may, or may not, cause problems. You could do lots of tests but the diodes are cheap.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sunnyiut
    0 sunnyiut over 10 years ago in reply to peterjcs23

    Thank you Peter,

    you are right, I don't need the protection diodes for my scheme [+5,0,-5].

    I have checked it out in practical, and it works fine.