Power & Energy
  • Technologies
  • More
Power & Energy
Forum Isolated DC-DC converters in series
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 282 subscribers
  • Views 1808 views
  • Users 0 members are here
  • series
  • dc_dc_converter
Related

Isolated DC-DC converters in series

sunnyiut
sunnyiut over 10 years ago

Hello everyone,

I am using two wireless charging modules for powering my circuit. The receiver part has 5v DC DC buck converter and I would like to connect the output of two modules in series to form a +/- 5v dual supply.

imageimage

 

Is there any chance of damaging any of the converters if I directly connect these in series? I have found that VicroPower and SynQor suggest to use protection diode at the output. These diodes are for preventing back-feeding by load capacitance during turn-off, and assuring proper operation during start-up and dynamic loading. Also prevent the output from going negative if only one converter is operational [like in case of thermal shutdown of one converter].

high voltage outputimage

Now, as my DC DC converters are totally isolated at the input side [two separate coils], do I need to use those protection diodes?

  • Sign in to reply
  • Cancel
Parents
  • peterjcs23
    0 peterjcs23 over 10 years ago

    The vicor scheme looks different as it is a 0 to 10V output, where as you are proposing a +5..0..-5V scheme. The vicor scheme could end up with one output feeding through the other but your scheme will not do that. No need for diodes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • sunnyiut
    0 sunnyiut over 10 years ago in reply to peterjcs23

    Thank you Peter,

    you are right, I don't need the protection diodes for my scheme [+5,0,-5].

    I have checked it out in practical, and it works fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • sunnyiut
    0 sunnyiut over 10 years ago in reply to peterjcs23

    Thank you Peter,

    you are right, I don't need the protection diodes for my scheme [+5,0,-5].

    I have checked it out in practical, and it works fine.