Power & Energy
  • Technologies
  • More
Power & Energy
Forum DC Lighting in an AC system
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 283 subscribers
  • Views 532 views
  • Users 0 members are here
  • dc/dc
  • lighting;
Related

DC Lighting in an AC system

e14 Contributor
e14 Contributor over 10 years ago

I currently have a small house that used to be on the grid but now we've taken it off.  There is a lighting system already set up and it's meant for AC bulbs.  A solar system is already set up with a 24 V battery bank and I want to run the lights off a DC power supply.  Do I have to change the configuration of the lighting set up to make the lighting work for DC or can i just put DC bulbs into the old sockets and attach the system to the 24V DC system.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    You can convert to ac 100W 24VDC to 24VAC Modified Sine Inverter and then step up to 120v But to use existing wiring old wiring would need to be replaced and be limited in distance depending on gauge  wire used.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    You can convert to ac 100W 24VDC to 24VAC Modified Sine Inverter and then step up to 120v But to use existing wiring old wiring would need to be replaced and be limited in distance depending on gauge  wire used.

    Clem