Power & Energy
  • Technologies
  • More
Power & Energy
Forum DC Lighting in an AC system
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 283 subscribers
  • Views 533 views
  • Users 0 members are here
  • dc/dc
  • lighting;
Related

DC Lighting in an AC system

e14 Contributor
e14 Contributor over 10 years ago

I currently have a small house that used to be on the grid but now we've taken it off.  There is a lighting system already set up and it's meant for AC bulbs.  A solar system is already set up with a 24 V battery bank and I want to run the lights off a DC power supply.  Do I have to change the configuration of the lighting set up to make the lighting work for DC or can i just put DC bulbs into the old sockets and attach the system to the 24V DC system.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 10 years ago

    You could use the old wiring for DC but the current rating may be a problem - if you can get 24V LED bulbs the increased efficiency should mean that the current rating of the wire should be OK (but you need to check). You also need to make very sure that the now 24V circuit can NEVER be connected to mains.

    Almost certainly you would do better to get a  24V -> mains converter - these are readily obtainable and quite cheap.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 10 years ago

    You could use the old wiring for DC but the current rating may be a problem - if you can get 24V LED bulbs the increased efficiency should mean that the current rating of the wire should be OK (but you need to check). You also need to make very sure that the now 24V circuit can NEVER be connected to mains.

    Almost certainly you would do better to get a  24V -> mains converter - these are readily obtainable and quite cheap.

     

    MK