Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging with low power
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 25 replies
  • Answers 4 answers
  • Subscribers 287 subscribers
  • Views 4617 views
  • Users 0 members are here
  • charging
  • battery_charger
  • low_power
  • battery
  • lipo
  • wireless
  • coil
  • tesla_coil
  • low_power_charger
  • low_power_supply
Related

Charging with low power

balearicdynamics
balearicdynamics over 10 years ago

If I charge a LiIon 500 mA 3.7 V battery with a charger that has a 100 mA power only, the battery will be charged in a longer time or not charged at all ?

 

Thanks in advance to solve this doubt.

 

Enrico

  • Sign in to reply
  • Cancel

Top Replies

  • amgalbu
    amgalbu over 10 years ago +3 suggested
    The charge processo of a LiPo battery has two phases Constant current: the voltage is kept to 4.2 V and current flows into the battery. The charger tries to keep current constant Constante voltage: when…
  • jonivanart
    jonivanart over 10 years ago in reply to balearicdynamics +1
    ambrogio is correct on the requirements the charger should be able to meet. I kinda got all technical on my answer so I hope it wasn't too confusing. LOL! Please mark a good answer if it was answered correctly…
  • crjeder
    crjeder over 10 years ago in reply to jonivanart +1
    Balancing is only needed when multiple cells are charged. This is because a cell which is carged to a lower voltage is the charged by an other cell with higher voltage and the current is not limited. A…
Parents
  • jc2048
    0 jc2048 over 10 years ago

    This is a Panasonic document that outlines how to do charging of lithium ion batteries:

     

    https://eu.industrial.panasonic.com/sites/default/pidseu/files/downloads/files/li-ion_handbook_22_10_15.pdf

     

    If there's no temperature monitoring of the cell, you wouldn't try to charge (for the constant current phase) at more than 0.5 to 0.7C, though that would depend on the situation of the battery (if it were wrapped in expanded foam you might want to measure the temperature and make sure it wasn't getting too hot). Charging and discharging are both exothermic (some of the energy going in during charging or coming out during discharge ends up as heat in the battery).

     

    Charging at a lower current will just take longer.

     

    Ambrogio perhaps could have added a third state. As well as the constant current and constant voltage phases, the charger needs to know when to stop. That can be done in a variety of ways, but the most usual is to stop when the current falls to a percentage of the C rate - the Panasonic document gives the range 7%-10%, which in the case of Enricho's 500mAh battery is between  35mA and 50mA. If you don't stop, but try to trickle charge it like a lead-acid battery, you'll overcharge the cell. There's some leeway, the manufacturer includes a chemical buffer that means you can go beyond the 100% capacity point without damage, but go too far beyond and you'll seriously degrade the cell. If you can get the data on the charger, look at the data for the end point and see if it's reasonable. If you can't get the data, you maybe could try charging the cell and measuring to see at what current the charging stops (and stop it yourself if it goes on too long, obviously), but you'd need a means of doing that that didn't interfere with the charging; an ordinary handheld meter on a current range has a high enough voltage drop that it interferes with the charging - some of the better bench meters could do this, but you probably don't own one.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 10 years ago

    This is a Panasonic document that outlines how to do charging of lithium ion batteries:

     

    https://eu.industrial.panasonic.com/sites/default/pidseu/files/downloads/files/li-ion_handbook_22_10_15.pdf

     

    If there's no temperature monitoring of the cell, you wouldn't try to charge (for the constant current phase) at more than 0.5 to 0.7C, though that would depend on the situation of the battery (if it were wrapped in expanded foam you might want to measure the temperature and make sure it wasn't getting too hot). Charging and discharging are both exothermic (some of the energy going in during charging or coming out during discharge ends up as heat in the battery).

     

    Charging at a lower current will just take longer.

     

    Ambrogio perhaps could have added a third state. As well as the constant current and constant voltage phases, the charger needs to know when to stop. That can be done in a variety of ways, but the most usual is to stop when the current falls to a percentage of the C rate - the Panasonic document gives the range 7%-10%, which in the case of Enricho's 500mAh battery is between  35mA and 50mA. If you don't stop, but try to trickle charge it like a lead-acid battery, you'll overcharge the cell. There's some leeway, the manufacturer includes a chemical buffer that means you can go beyond the 100% capacity point without damage, but go too far beyond and you'll seriously degrade the cell. If you can get the data on the charger, look at the data for the end point and see if it's reasonable. If you can't get the data, you maybe could try charging the cell and measuring to see at what current the charging stops (and stop it yourself if it goes on too long, obviously), but you'd need a means of doing that that didn't interfere with the charging; an ordinary handheld meter on a current range has a high enough voltage drop that it interferes with the charging - some of the better bench meters could do this, but you probably don't own one.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer