Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging with low power
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 25 replies
  • Answers 4 answers
  • Subscribers 287 subscribers
  • Views 4617 views
  • Users 0 members are here
  • charging
  • battery_charger
  • low_power
  • battery
  • lipo
  • wireless
  • coil
  • tesla_coil
  • low_power_charger
  • low_power_supply
Related

Charging with low power

balearicdynamics
balearicdynamics over 10 years ago

If I charge a LiIon 500 mA 3.7 V battery with a charger that has a 100 mA power only, the battery will be charged in a longer time or not charged at all ?

 

Thanks in advance to solve this doubt.

 

Enrico

  • Sign in to reply
  • Cancel

Top Replies

  • amgalbu
    amgalbu over 10 years ago +3 suggested
    The charge processo of a LiPo battery has two phases Constant current: the voltage is kept to 4.2 V and current flows into the battery. The charger tries to keep current constant Constante voltage: when…
  • jonivanart
    jonivanart over 10 years ago in reply to balearicdynamics +1
    ambrogio is correct on the requirements the charger should be able to meet. I kinda got all technical on my answer so I hope it wasn't too confusing. LOL! Please mark a good answer if it was answered correctly…
  • crjeder
    crjeder over 10 years ago in reply to jonivanart +1
    Balancing is only needed when multiple cells are charged. This is because a cell which is carged to a lower voltage is the charged by an other cell with higher voltage and the current is not limited. A…
Parents
  • crjeder
    0 crjeder over 10 years ago

    By reading a bit more I'd say probably you can charge as long as you can provide a voltage of around 4,2 V. The switchover from constant current to constant voltage might not happen, which leaves you with a battery charged only 75 - 80 %. (if I understand this correctly)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • crjeder
    0 crjeder over 10 years ago in reply to crjeder

    I was not correct, the switchover would happen, but the constant voltage phase might end to early. This is because it ends when the current drops under a threshhold level which might be higher than the provided current. My conclusion was correct, though. The battery might not be charged to it's full capacity.

     

    So my answer would be this:

     

    "Yes, it is possible to charge a battery with a current far less than 1 C, but it might not be charged to it's full capacity"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to crjeder

    Hello,

     

    this impact with my initial implied assumption. I see that there are many charger that provide a lower power than the battery power, especially in smartphones and tablets. The same USB charger working on 500 mA full charge a 1500 mA battery. Some ideas what I am seeing under the bad perspective?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to crjeder

    Hello,

     

    this impact with my initial implied assumption. I see that there are many charger that provide a lower power than the battery power, especially in smartphones and tablets. The same USB charger working on 500 mA full charge a 1500 mA battery. Some ideas what I am seeing under the bad perspective?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • crjeder
    0 crjeder over 10 years ago in reply to balearicdynamics

    True, many SmartPhones / Tablets would charge at 1/3 C to 1/12 C. Or in other words 500 mA are 1/3 of 1500 mAh and 1/6 of 6600 mAh (IPad)

    But if you provide the IPad charger with something lower than 500 mAh (say 300 mA for example) than it would trigger the end of the "constant voltage" charging phase immediatly because 5 % C is just 330 mA. This is below the above mentioned (by jc2048) 7 - 10 % C.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to crjeder

    Hey Crjeder!

     

    finally I am - slowly I admit - reaching the solution with the help of all. What you say is true. So, with the following parameters:

     

    Battery: 3.7V 500 mA

    Charger> same voltage (with a limiting resistor) and 100 mA

     

    as the charger is 1/5C should I expect that it triggers correctly when the battery is charged? (that is between your example of 1/3 and 1/6) image

     

    Enrico