Power & Energy
  • Technologies
  • More
Power & Energy
Forum Powering a sega cdx with rechargeable batteries
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 284 subscribers
  • Views 1373 views
  • Users 0 members are here
Related

Powering a sega cdx with rechargeable batteries

e14 Contributor
e14 Contributor over 10 years ago

So thanks in advance for your help with this! I'm trying to power a Sega cdx off of some 9.6v rechargeable NiMH batteries using one end of a broken Sega ac adapter. The cdx ac adapter outputs 9.5v@1.5A and the batteries are 9.6v with a 2000 mah capacity.

I have almost no knowledge about this and can't figure out why it doesn't power on so any help is appreciated!

 

Oh I found out Ben Heck did this in one of his early podcasts but I would like to keep my cdx as is lol

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 10 years ago

    Hi Rhysthekeen,

    Are you sure you have the + of the battery on the same pole of the adapter as the + of the AC adapter. Does the AC adapter indicate that the output is DC. This may be a graphic that looks like a long line over 3 dashes. If the poles are matched and the adapter has a DC output the battery should work. 9.6 Volts and 9.5 Volts are compatible in this application.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jw0752

    As certain as I can be without  a multimeter which comes tomorrow. The ac adapter outputs 9.5v DC @ 1.5 A. The cable is positive inside negative and consists of 2 groups of copper wires, one wrapped in green plastic sheath which should be the positive and the rest spread around without any sheath. I take this to be the negative?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jw0752

    As certain as I can be without  a multimeter which comes tomorrow. The ac adapter outputs 9.5v DC @ 1.5 A. The cable is positive inside negative and consists of 2 groups of copper wires, one wrapped in green plastic sheath which should be the positive and the rest spread around without any sheath. I take this to be the negative?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Hi,

    What you say makes sense. You should be able to confirm when your meter arrives. The amperage rating on the battery and power supply are only there to give you an indication of the upper limit of power available under suitable load. Let me know what you find out. I would start by measuring the voltage of the battery to confirm it is in good condition and charged.

    John