Power & Energy
  • Technologies
  • More
Power & Energy
Forum Convert 12V 200mA to 5V 450mA
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 286 subscribers
  • Views 1501 views
  • Users 0 members are here
  • smps
  • ac-dc power supply
Related

Convert 12V 200mA to 5V 450mA

rishi2628
rishi2628 over 9 years ago

I am making a transformer-less AC to Dc power supply and the best design that I have got till now is this:-

 

image

 

For better understanding you can download this PDF:-

www.nxp.com/documents/user_manual/UM10522.pdf

 

This circuit uses a TEA1721 ic to convert AC Mains voltage to DC voltage. This design claims to have a 77% efficiency without a transformer and is non-isolated, both of which are fine by me.

 

The output of this converter is 12V 200mA and I desire 5V 450mA (or greater amperage). Please suggest any changes that I can make in this circuit to get a 5V 450mA output.

 

If there is a better circuit (without any transformer) which has a better efficiency and an output of 5V 500mA (or greater amperage), then please do suggest me that as well.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago +3 suggested
    This will sound rude and I'm sorry, but if you need to ask this question you should not be trying to build a transformerless mains to 5V converter - unless such devices are used under carefully controlled…
  • bob_u
    bob_u over 9 years ago +3 suggested
    Look at Power Integrations LinkSwitch TN family. These ICs are made for wide range AC to DC buck converters. PI has good app notes. As others have commented, be careful, there's no isolation. It's very…
  • michaelkellett
    michaelkellett over 9 years ago in reply to rishi2628 +2 suggested
    For small numbers then buy a ready made remotely switchable power socket like this: https://www.amazon.co.uk/Status-SREMSOC-Remote-Control-Socket/dp/B007Y7D8Z6/ref=sr_1_1?ie=UTF8&qid=1481454332&sr=8-1&key…
Parents
  • michaelkellett
    0 michaelkellett over 9 years ago

    This will sound rude and I'm sorry, but if you need to ask this question you should not be trying to build a transformerless mains to 5V converter - unless such devices are used under carefully controlled conditions they are very dangerous.

     

    What do you need the power supply for - perhaps someone can suggest  a better or safer solution.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 9 years ago

    This will sound rude and I'm sorry, but if you need to ask this question you should not be trying to build a transformerless mains to 5V converter - unless such devices are used under carefully controlled conditions they are very dangerous.

     

    What do you need the power supply for - perhaps someone can suggest  a better or safer solution.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer