Power & Energy
  • Technologies
  • More
Power & Energy
Forum Why is my LTC3780 only giving 0.8V - 2.8V output?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 283 subscribers
  • Views 3725 views
  • Users 0 members are here
  • lct3780
Related

Why is my LTC3780 only giving 0.8V - 2.8V output?

tim687
tim687 over 9 years ago

Recently I bought two of these, I was needed to remove all of the pots since they where bad. I soldered a resistor (500K) like this to the board to make sure that the undervoltage protection won't go off, since that was the issue I had when I powered up the board for the first time. That issue caused the fault led to light up and the output to not work.

I got one board working, since I wanted to get one working before I changed the other one. I am not sure if the resistor fix is correct here.

image

 

Now, a few days (maybe weeks further), I continued with the project and tried a reverse polarity protection circuit. That didn't work very well, but it was fun to see something, that is not supposed to light up, light up (@28.5V). Everything continued to work after the short!


The next day I soldered the banana plugs that came in to the output wires and all of a sudden the device wouldn't power more than around 2.8V. The fault led is lighting up and the chip is getting very hot.

 

Did I blew up the chip by testing out the lighting effects on components?

 

The strange thing is that, the other board isn't working at all. Same problem as the first one.

I didn't test the shortcut capabilities of the second board though.

 

I have ordered two new LTC3780's and a few of the LM358N's to make sure that they are all good.

 

 

I am doing anything wrong?

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 9 years ago

    What is the LM358 doing - do you have a schematic for this board ?

     

    I'd need to see that before I could suggest things to measure - what test gear have you got (it affects what I might suggest checking) ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tim687
    0 tim687 over 9 years ago in reply to michaelkellett

    I think it's for the power cut off circuitry. I found this link that explains it. It also contains a partial schematic.

    I only got a multimeter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelwylie
    0 michaelwylie over 9 years ago in reply to tim687

    Check to make sure none of those solder joints are shorted to a pin adjacent. Use the continuity checker on your multimeter. If you don't have a continuity checker, use the ohm meter to check for 0 resistance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to tim687

    I think you should trace out the board to work out exactly how that extra chip is connected. You can just connect the 3780's run pin with a resistor - op-amps aren't needed.

     

    Before changing anything it would nice to know the supply current being drawn and the voltage measured on all the 3780 pins.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to tim687

    I think you should trace out the board to work out exactly how that extra chip is connected. You can just connect the 3780's run pin with a resistor - op-amps aren't needed.

     

    Before changing anything it would nice to know the supply current being drawn and the voltage measured on all the 3780 pins.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • tim687
    0 tim687 over 9 years ago in reply to michaelkellett

    0.17A @ 12 V. I'll check the voltage tomorrow