Power & Energy
  • Technologies
  • More
Power & Energy
Forum Power Supply Question and Request.
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 5 answers
  • Subscribers 284 subscribers
  • Views 2202 views
  • Users 0 members are here
  • power regulator
  • power electronics
  • power design
Related

Power Supply Question and Request.

eye-zen
eye-zen over 8 years ago

Hi People - i have a request for the members for assistance.

Brief Background - I build Robots and Drones - both ground based and aerial. My background is programming not physical design....

 

My request is this:-

A power circuit capable of taking in at least 36v dc and outputting any and or all of the following 3,3v 5v 6v 7.4v 9v 10v 12v -- these are the standqrd voltages required by our robotics platforms.

The input voltage needs to be anywhere from 6v to at least 36v - although higher is ok.

 

The out[uts would ideally be switchable and selectable so that at least any 3 of those voltages could be output at once - ie 3.3 and 5 and 10 volts out all at once....

 

I dont know if this is possible or not - thats where you come in ....

If possible i would like a schematic and a BOM to build this..

 

Please help

Cheers

Al

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +5 suggested
    Hi Al, What you describe is possible, but to build a universal supply will not be as efficient as building to a specification. For a specific application one would need to know the voltage of the source…
  • rachaelp
    rachaelp over 8 years ago in reply to eye-zen +3
    Al French wrote: ahhh and also ltpowercad looks like a windoze program - why doesnt anyone support linux anymore hahaha - virtualbox here we come Tell me about it.... I use Mac/Linux machines and Windows…
  • dougw
    dougw over 8 years ago +1 suggested
    You could try one of the design tools that guide you through complete solutions. Like TI tools: Power supply design for single loads | WEBENCH tools | TI.com SWITCHERPRO SwitcherPro(TM) Switching Power…
Parents
  • jw0752
    0 jw0752 over 8 years ago

    Hi Al,

    If some of your circuits require less than 1 A there is a nice series of DC to DC converters from Recom. They will convert up to 28 volts in to fixed 3.3 V, 5 V, 9 V, 12 V, and 15V, at 1 amp and do it with nearly 90% efficiency so there is no a need for a lot of heat sinking. Further they are quite small. Here is a link to the 5 volt unit.

     

    http://www.newark.com/recom-power/r-78e5-0-1-0/dc-dc-converter-5w-5v-1a-sip/dp/83X9336?ost=R-78E5.0-1.0&scope=partnumberlookahead&exaMfpn=true&searchref=searchlookahead&searchView=table&iscrfnonsku=false&ddkey=http%3Aen-US%2FElement14_US%2Fw%2Fsearch

     

    If you want more than one Amp then it will require extra work. I suspect that one could put in the support hardware for the higher amperage output and perhaps use the little DC to DC converters as Plug in voltage selectors to drive the components that would deliver the higher amperage.

     

    You might note that while you will get questions answered and a lot of help on the forum it is unlikely that anyone will design the circuit for you. For one thing there may be liability issues if something that is designed fails and property is damaged or people are hurt. Some of the guys on the forum do circuit designs for a living and you may be able to contract with one of them to do your design for you but they will have to speak for themselves. I personally do not have the skills yet to take on a design project for someone other than myself. If you can find the resources to start designing and prototyping the board that you want I am sure that there will be help with the bumps in the road from the guys here.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • eye-zen
    0 eye-zen over 8 years ago in reply to jw0752

    hi mate

    Liability is something i am aware of - and would not hold anyone here giving me assistance liable for anything except credit where credit is due....

    i am far from a litigious person -

    I am only hoping i can find the solution we require for our design ...

    Having said that maybe there is already enough info for us to progress -

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • eye-zen
    0 eye-zen over 8 years ago in reply to jw0752

    hi mate

    Liability is something i am aware of - and would not hold anyone here giving me assistance liable for anything except credit where credit is due....

    i am far from a litigious person -

    I am only hoping i can find the solution we require for our design ...

    Having said that maybe there is already enough info for us to progress -