Power & Energy
  • Technologies
  • More
Power & Energy
Forum Power Supply Question and Request.
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 5 answers
  • Subscribers 284 subscribers
  • Views 2223 views
  • Users 0 members are here
  • power regulator
  • power electronics
  • power design
Related

Power Supply Question and Request.

eye-zen
eye-zen over 8 years ago

Hi People - i have a request for the members for assistance.

Brief Background - I build Robots and Drones - both ground based and aerial. My background is programming not physical design....

 

My request is this:-

A power circuit capable of taking in at least 36v dc and outputting any and or all of the following 3,3v 5v 6v 7.4v 9v 10v 12v -- these are the standqrd voltages required by our robotics platforms.

The input voltage needs to be anywhere from 6v to at least 36v - although higher is ok.

 

The out[uts would ideally be switchable and selectable so that at least any 3 of those voltages could be output at once - ie 3.3 and 5 and 10 volts out all at once....

 

I dont know if this is possible or not - thats where you come in ....

If possible i would like a schematic and a BOM to build this..

 

Please help

Cheers

Al

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +5 suggested
    Hi Al, What you describe is possible, but to build a universal supply will not be as efficient as building to a specification. For a specific application one would need to know the voltage of the source…
  • rachaelp
    rachaelp over 8 years ago in reply to eye-zen +3
    Al French wrote: ahhh and also ltpowercad looks like a windoze program - why doesnt anyone support linux anymore hahaha - virtualbox here we come Tell me about it.... I use Mac/Linux machines and Windows…
  • dougw
    dougw over 8 years ago +1 suggested
    You could try one of the design tools that guide you through complete solutions. Like TI tools: Power supply design for single loads | WEBENCH tools | TI.com SWITCHERPRO SwitcherPro(TM) Switching Power…
Parents
  • eye-zen
    0 eye-zen over 8 years ago

    image

     

    So this is where im at so far - and it looks like it might work for me - just need to work out the BOM and then see how feasible it is size and cost wise.. thanks everyone for your input and assistance..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 8 years ago in reply to eye-zen

    Al, your first post mentions input from 6 to 36 V.

    Some of your desired outputs are higher than 6 V. I it's a requirement to have outputs that can be lower as well as higher than the input, a Buck design will not do. A Buck-boost design can handle that.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 8 years ago in reply to eye-zen

    Al, your first post mentions input from 6 to 36 V.

    Some of your desired outputs are higher than 6 V. I it's a requirement to have outputs that can be lower as well as higher than the input, a Buck design will not do. A Buck-boost design can handle that.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer