Power & Energy
  • Technologies
  • More
Power & Energy
Forum Battery choice advise for College project needed
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 28 replies
  • Answers 19 answers
  • Subscribers 285 subscribers
  • Views 3638 views
  • Users 0 members are here
Related

Battery choice advise for College project needed

bionicle_159
bionicle_159 over 8 years ago

I’m making a project for college and am having trouble incorporating the huge size of the battery compartment, are there any alternatives I could use to 3x AA power (4.5 volts)? I’ve looked at button cell equivalents but I’m not well versed in substituting voltages and milliamps. Thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +5 suggested
    You can get 3.9 - 4.2 V from a small rectangular Lithium polymer battery. There are also Lithium "button" cells available, but usually only 3V. What are you running from these batteries? - very few devices…
  • dougw
    dougw over 8 years ago in reply to bionicle_159 +4 suggested
    When they say don't use NiCad or NiMH it usually means their voltage is too low, so your device probably works better above 4 V. I would expect 5 V is okay as well given the tolerance on alkaline batteries…
  • beacon_dave
    beacon_dave over 8 years ago in reply to jw0752 +4 suggested
    Sounds about right. I have found that the mAh rating is usually based upon the battery inside (e.g. 3.7v) and not on the USB 5v output. I was looking for one closer to 3,500mAh in this case to match the…
Parents
  • beacon_dave
    0 beacon_dave over 8 years ago

    Perhaps you could give some more information on the requirements ?

     

    3x AAA

    3x AAAA

    3x N

    are all smaller but they will trade size for capacity.

     

    The N type is about half the size of the AA but about one third the capacity.

    608306 ENERGIZER, Battery, Single Cell, 1.5 V, N, Alkaline, 900 mAh, Raised Positive and Flat Negative, 12 mm | Farnell …

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bionicle_159
    0 bionicle_159 over 8 years ago in reply to beacon_dave

    I’ll have to check tomorrow when I’m back with my equipment at college, the included sheets with the arcade have left nothing about what current or precice minimal voltage it operates at, it does however say to not use Nickel Cadmium or any other rechargable batteries for whatever reason, perhaps it outputs some low level enegy that could interfere.

    It operates with 3x AA so i presume its maximum voltage it can accept is 4.5v. I’d need to order some of the suggested battery compartments to try and see if they’d fit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to bionicle_159

    A simple test with an ammeter will give you an indication of what current it draws when powered up.

     

    The NiCd rechargeable batteries typically only have a voltage rating of 1.2v per cell so would drop your 4.5v down to 3.6v.

     

    What sort of reduction in size are you looking for ?

     

    Also what sort of capacity do you require ? Do the AA batteries (at around 2700mAh) currently just provide enough duration ? could you make do with less duration in favour of compactness ?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bionicle_159
    0 bionicle_159 over 8 years ago in reply to beacon_dave

    I’ve got a case size with a height of 12cm and width of 10cm and a base of around 4-5cm, I need to fit a screen in at around 55 degree angle, perhaps I could try and fit the batteries in the lower half (4cm) but that is assuming that the circuit board for the controls do not occupy the area. I’d like to also fit the beeper at the same time so that might need to be placed elsewhere if it conflicts. Since it’s a portable product I’d like to still have a sufficient enough duration of power but would definitely want the physical size benefits, like the N battery provide for example, in a compact product that mine is.

     

    I just checked the rechargeable battery i used again and the Ni-Cad battery was actually a Nickel Metal Hydride rated at 2000mAH, as mentioned previously they drained quite quickly but I might need to do another test to be fully sure that it was the electronics that caused the short time of power.

     

    Is it easy to acquire the compartments for the batteries you mentioned, I live in the UK but might be able to find such things at a general hardware store if the items are widely available.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bionicle_159
    0 bionicle_159 over 8 years ago in reply to bionicle_159

    Just realised what you meant with the 1.2v, yeah that’s probably what the issue was. Is Alkaline the best option to use or do other types need some looking into?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to bionicle_159

    1.2v at 2000mAh is significantly less capacity compared to a typical alkaline rated at 1.5v at 2700mAh so not surprising that they appear to drain quite quickly. However you need to look at the data sheets as the performance varies depending upon load, which means you need to check your current draw in normal use.

     

    Not sure if anyone is doing a lithium in N type package, however Energizer do a AAA sized one:

    http://data.energizer.com/pdfs/l92.pdf

    which is slightly smaller than AA but significantly less performance than their AA version:

    http://data.energizer.com/pdfs/l91.pdf

     

    Farnell is a UK based company, and they have some N type battery holders listed. Not sure if your college has an account with Farnell. If not then their sister company CPC will sell to individuals.

    http://cpc.farnell.com/pro-power/25vb11d/battery-holder-1xn-solder-tag/dp/BT03697

     

    You could try Maplin, or Mouser or Amazon.co.uk etc...

     

    You could also make your own holder using these PCB style terminals:

    http://cpc.farnell.com/keystone/590/battery-holder-aa-n-1-way/dp/BT04910

    which may be advantageous as you could fit the batteries in the spaces you have available around other parts rather than having to make room for a bulky holder.

     

    Presumably your college will have access to 3D printing facilities by now allowing you to be very creative with component mounting. With 120mm of height then you could consider stacking 3x N-type vertically in series in one corner of the case and then in parallel with the same again in the opposite corner to increase capacity.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to bionicle_159

    When they say don't use NiCad or NiMH it usually means their voltage is too low, so your device probably works better above 4 V. I would expect 5 V is okay as well given the tolerance on alkaline batteries.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 8 years ago in reply to bionicle_159

    When they say don't use NiCad or NiMH it usually means their voltage is too low, so your device probably works better above 4 V. I would expect 5 V is okay as well given the tolerance on alkaline batteries.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • bionicle_159
    0 bionicle_159 over 8 years ago in reply to dougw

    Well it’s not the type of product that I’d use everyday so I would agree with your thinking on the voltage tolerance of the device, I’d just like a standard alternative that in the event of it needing replacement, I can purchase again from a standard hardware store at most without having to pay out a considerable sum

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to bionicle_159

    The USB power packs jw0752 mentions are available anywhere, even Dollar Stores and are available in a wide variety of sizes.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bionicle_159
    0 bionicle_159 over 8 years ago in reply to dougw

    Okay I’ll be on the lookout for those, are there any websites that already have 3d printing designs for battery terminals available to the public, they’d save me a lot of time as I plan to have the model to be able to be dismantled especially since I plan to use the electronics in a final prototype, using screws over gluing the electronics in place

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to bionicle_159

    ...are there any websites that already have 3d printing designs for battery terminals available to the public...

    Perhaps try a search for 'battery holder' on Thingiverse

    https://www.thingiverse.com/

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bionicle_159
    0 bionicle_159 over 8 years ago in reply to beacon_dave

    Hi, I had a look but couldn‘t seem to find one for the N battery, the only ones that came up were the smaller sized 12v batteries. I think I’ll just glue the holders together as the N battery seems to be rarely used in comparison. I‘ll get back to you guys once I work out how this is gonna fit together. Hope you guys have a nice week image