Power & Energy
  • Technologies
  • More
Power & Energy
Forum Battery choice advise for College project needed
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 28 replies
  • Answers 19 answers
  • Subscribers 285 subscribers
  • Views 3647 views
  • Users 0 members are here
Related

Battery choice advise for College project needed

bionicle_159
bionicle_159 over 8 years ago

I’m making a project for college and am having trouble incorporating the huge size of the battery compartment, are there any alternatives I could use to 3x AA power (4.5 volts)? I’ve looked at button cell equivalents but I’m not well versed in substituting voltages and milliamps. Thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +5 suggested
    You can get 3.9 - 4.2 V from a small rectangular Lithium polymer battery. There are also Lithium "button" cells available, but usually only 3V. What are you running from these batteries? - very few devices…
  • dougw
    dougw over 8 years ago in reply to bionicle_159 +4 suggested
    When they say don't use NiCad or NiMH it usually means their voltage is too low, so your device probably works better above 4 V. I would expect 5 V is okay as well given the tolerance on alkaline batteries…
  • beacon_dave
    beacon_dave over 8 years ago in reply to jw0752 +4 suggested
    Sounds about right. I have found that the mAh rating is usually based upon the battery inside (e.g. 3.7v) and not on the USB 5v output. I was looking for one closer to 3,500mAh in this case to match the…
Parents
  • jw0752
    0 jw0752 over 8 years ago

    Hi,

    I have found using a small cell phone recharger module useful for situations like this. You can recharge it with a standard mini USB 5 volt charger and it has an output of a regulated 5 volts. I has more capacity than 3 AA batteries and has a similar volume.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bionicle_159
    0 bionicle_159 over 8 years ago in reply to jw0752

    Hi, I’m not sure if the device will accept it as it says in the manual not to use rechargable batteries in general, I tried using standard rechargable Ni-Cads to see if there was any reason and they drained pretty quickly within about 2-3 hours. I’m concerned if the battery outputting 5v will cause long-term harm to the device as I’ve had past experience of CD players using the weird 4.5v rating that have overheated after extended use with 5v PSUs

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to bionicle_159

    Fresh AA Alkaline batteries will start at about 1.6V which is 4.8 Volts for three. The nice thing about the cell phone rechargers are that they have a small boost DC to DC converter incorporated that keeps the output at 5 volts down to the shut down discharge level of the lithium batteries. Another advantage to lithium is the thin profile of many of the cells. I am not trying to sell this as a solution but it is worth a consideration.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bionicle_159
    0 bionicle_159 over 8 years ago in reply to jw0752

    Sure, do you know how much are they usually priced at and if they are easy to find on general hardware/electronic stores and websites?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to bionicle_159

    How about this USB power bank for size/price:

    https://www.maplin.co.uk/p/maplin-2200mah-portable-powerbank-black-n39eq

     

    (Note that their stated dimensions appear to be out by a factor of 10, either that or they have very large credit cards...)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bionicle_159
    0 bionicle_159 over 8 years ago in reply to beacon_dave

    That one might be a good snug fit just behind the lcd. I can’t believe that with the premiums that Maplin charges, they still don’t think to use that money to hire someone to proofread their items. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to beacon_dave

    The empirical tests I have run on similar units indicate that if they claim 2200mAh one can realistically expect about 1500 mAh actual performance.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 8 years ago in reply to beacon_dave

    The empirical tests I have run on similar units indicate that if they claim 2200mAh one can realistically expect about 1500 mAh actual performance.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to jw0752

    Sounds about right. I have found that the mAh rating is usually based upon the battery inside (e.g. 3.7v) and not on the USB 5v output. I was looking for one closer to 3,500mAh in this case to match the alkaline AA capacity but they tend to jump up in size dramatically.

     

    However as you've mentioned previously, they do tend to hold their output voltage better than the drop off of a battery which may help in certain applications.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer