Power & Energy
  • Technologies
  • More
Power & Energy
Forum Battery choice advise for College project needed
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 28 replies
  • Answers 19 answers
  • Subscribers 284 subscribers
  • Views 3669 views
  • Users 0 members are here
Related

Battery choice advise for College project needed

bionicle_159
bionicle_159 over 8 years ago

I’m making a project for college and am having trouble incorporating the huge size of the battery compartment, are there any alternatives I could use to 3x AA power (4.5 volts)? I’ve looked at button cell equivalents but I’m not well versed in substituting voltages and milliamps. Thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +5 suggested
    You can get 3.9 - 4.2 V from a small rectangular Lithium polymer battery. There are also Lithium "button" cells available, but usually only 3V. What are you running from these batteries? - very few devices…
  • dougw
    dougw over 8 years ago in reply to bionicle_159 +4 suggested
    When they say don't use NiCad or NiMH it usually means their voltage is too low, so your device probably works better above 4 V. I would expect 5 V is okay as well given the tolerance on alkaline batteries…
  • beacon_dave
    beacon_dave over 8 years ago in reply to jw0752 +4 suggested
    Sounds about right. I have found that the mAh rating is usually based upon the battery inside (e.g. 3.7v) and not on the USB 5v output. I was looking for one closer to 3,500mAh in this case to match the…
  • bionicle_159
    0 bionicle_159 over 8 years ago in reply to beacon_dave

    That one might be a good snug fit just behind the lcd. I can’t believe that with the premiums that Maplin charges, they still don’t think to use that money to hire someone to proofread their items. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to beacon_dave

    The empirical tests I have run on similar units indicate that if they claim 2200mAh one can realistically expect about 1500 mAh actual performance.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to jw0752

    Sounds about right. I have found that the mAh rating is usually based upon the battery inside (e.g. 3.7v) and not on the USB 5v output. I was looking for one closer to 3,500mAh in this case to match the alkaline AA capacity but they tend to jump up in size dramatically.

     

    However as you've mentioned previously, they do tend to hold their output voltage better than the drop off of a battery which may help in certain applications.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to bionicle_159

    The Adafruit Powerboost might be another option:

    https://www.adafruit.com/product/1944

    https://www.adafruit.com/product/2465

     

    It would allow you to size the battery based on space / capacity requirements, like this 2500mAh one:

    https://www.adafruit.com/product/328

     

    Perhaps not the cheapest option however.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • luislabmo
    0 luislabmo over 8 years ago in reply to bionicle_159

    Some manufacturers recommend not to use rechargeable batteries not because is a technical restriction (most of the times), it will be to stop giving false impression to the user that the device in question doesn't work according to the specs (like duration of batteries). You can see this in some flashlights where you can use rechargeable batteries but their brightness/duration won't be the same as when using Alkaline. -my 2 cents-. How about using a USB charger as suggested by others and use an adjustable switching regulator?

     

    Luis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to luislabmo

    I've also seen the "don't use rechargable batteries" because it has no ability to recharge, and the current available from rechargables can cause issues if there is a component failure.

    Generally the normal batteries simply discharge.

     

    I was talking with a teacher about Edison Robots ( https://meetedison.com/  ) and he showed me that the battery connections were the weak point.

    However he was using rechargable batteries, and when I explained the issues with current and that pupils could stall them, etc, it made sense why they were overloading the connections, and having so many issues.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bionicle_159
    0 bionicle_159 over 8 years ago in reply to bionicle_159

    Hi, sorry for the long wait, I’ve been ill and the multimeter at the school was broken, I managed to borrow an ammeter from science and here’s the readings:

    peak reading: 4.19A

    steadiest reading ~ 3.60A

     

    Thoughts:

    The arcade would keep resetting when I tried to get a reading off the board, the batteries also felt quite warm after I finished, I think it might have been reading more than it necessarily needed as the ammeter was intercepting the circuit, requiring more energy needed for the arcade.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to bionicle_159

    The ammeter goes in series with the load. Sounds like you've placed it directly across the battery and shorted it out.

     

    BBC - KS3 Bitesize Science - Electric current and voltage : Revision, Page 5

     

     

    PS I spotted some compact USB power banks in Asda at the weekend - might be worth you taking a look at a store near you to see if there is anything that would work.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<