Power & Energy
  • Technologies
  • More
Power & Energy
Forum Supercapacitor Charging Circuit
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 4 answers
  • Subscribers 283 subscribers
  • Views 3267 views
  • Users 0 members are here
  • supercapacitor
Related

Supercapacitor Charging Circuit

aidamahn
aidamahn over 8 years ago

Greetings!

 

I have questions about a supercapacitor charging circuit that I hope the community can help answer.  I've included two of my schematics below. This circuit is to keep a Raspberry Pi 3 Model B running long enough to safely shutdown when power is cut.  I have an Arduino watching the input voltage presence and the voltage level coming from the supercaps. (Sorry for not including the voltage divider to the Arduino analog pin on the superconductor side, the resistors are 100K and 1M)

 

Essentially the Arduino waits for the the supercaps to charge up to 5 volts then toggles a solid state relay to turn on the RPi.  When the voltage is cut or it detects a bad voltage drop from the supercaps it tells the RPI to shutdown via a GPIO.  There is another GPIO line coming from the RPi that tells the Aruidno when the RPi is off so it can turn off the relay.

 

I have two 22F 2.7V superconductors in series to create 5.4V.  I have a 6V 2.5A DC power supply dialed down to 5.4V via 3A capable buck converter.

 

Here is the math I did to come up with the resistance needed in front of the supercaps to not nuke my power supply.  I also have two schottky diodes in series with the resistors.

 

5.4V / 2.5A = 2.16 Ohms

5.4V x 2.5A = 13.5W

 

Right now I have this charging up nicely and running the Arduino Uno for an impressive amount of time.

 

Questions:

 

  1. Currently I am using resistors in parallel, is that over kill?  It just felt good to me.
  2. What schottky diode would you recommend?  I am only using a 40V 5A diodes because that is what I have on hand.
  3. If I do need to use parallel resistors, do I need two schottkys or would one be enough?
  4. Do you think my supercaps will be enough?  I also have two 50F 2.7V in my parts bin.
  5. Anything else I am missing with this circuit?

 

Single resistor:

image

 

Parallel Resistors:

image

 

Message was edited by: Jeremy Morgan (added Raspberry Pi version)

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +8 suggested
    Hi Jeremy, I agree with what both John and Doug mention. The supercaps will store a lot of energy and the majority of that will be unused, because the voltage will drop to the point that the Pi won't operate…
  • dougw
    dougw over 8 years ago +6 suggested
    I don't have experience with these caps, but I might be tempted to use 2.7V zeners instead of those 100 ohm resistors.
  • jw0752
    jw0752 over 8 years ago +5 suggested
    Hi Jeremy, The series parallel resistors look like a bit of overkill. Your single 15 Watt resistor should handle any eventuality including a dead short across the capacitor. You may want to incorporate…
Parents
  • dougw
    0 dougw over 8 years ago

    I don't have experience with these caps, but I might be tempted to use 2.7V zeners instead of those 100 ohm resistors.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 8 years ago

    I don't have experience with these caps, but I might be tempted to use 2.7V zeners instead of those 100 ohm resistors.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • aidamahn
    0 aidamahn over 8 years ago in reply to dougw

    Thanks.  I just watched a EEVBlog video on zeners and understand why.

     

    Would these zeners work?

    http://www.newark.com/vishay/1n5223b-tr/zener-diode-500mw-2-7v-do-35/dp/18M3523

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to aidamahn

    Maybe not, the peak power is over 6 watts in the top zener.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • aidamahn
    0 aidamahn over 8 years ago in reply to dougw

    I think I might have found a better solution for the over voltage protection, the TL431.  It can be dialed to any voltage from 2.5V to 36V.  They appear to be used in the commercial supercapacitor protection boards.

     

    http://www.ti.com/lit/ds/symlink/tl431a.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to aidamahn

    Nice devices, but it looks like they can only handle 100 mA.