Power & Energy
  • Technologies
  • More
Power & Energy
Forum converting to 5V power supply
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 3 answers
  • Subscribers 283 subscribers
  • Views 1451 views
  • Users 0 members are here
Related

converting to 5V power supply

houandreas
houandreas over 8 years ago

Hi, I have a base board which offers 2.5V@8A, 3.3V@8A and 12V@1A power supply but my sister board need 5V. So I'm considering to convert 12V to 5V, can I just use two resistors (10k and 24k ohm) to do that? This is under assumption that the sister board's impedance is high so I'm not sure if this simple circuit works. It should work but I'm rly not sure.. first time for me doing this.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +6 suggested
    Hi Bin, The calculation is not right, you can use this web page to do it (the formula is there too): Voltage Divider Calculator However, unless your sister board has very low current requirement (much…
  • jw0752
    jw0752 over 8 years ago +5 verified
    Hi Bin, This little DC / DC converter will work well for your application. I have used them in similar applications. http://www.newark.com/recom-power/r-78e5-0-0-5/dc-dc-converter-2-5w-5v-0-5a-sip/dp/62X9499…
  • genebren
    genebren over 8 years ago +3 suggested
    Hi Bin, Both shabaz and jw0752 have offered some sound advice (as they are known to do around here). Another simple and perhaps lower cost approach might be a simple 5.0V regulator. This is feasible is…
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Bin,

     

    The calculation is not right, you can use this web page to do it (the formula is there too):

    Voltage Divider Calculator

    However, unless your sister board has very low current requirement (much less than the current through the resistors - you can type in the resistor value and the voltage at this page to find out the current, or just use Current=Voltage/Resistance : Ohms Law Calculator ) then the answer is you'll need something else, most likely a DC-DC converter. If you provide more information about the sister board, then it is possible to help more. Similarly, although you have not specified the base board (which makes it harder to help you again), it sounds like a computer power supply. If you are not going to use the other two outputs, then please confirm it will operate if you do not use the other two outputs at all because some older computer PSUs may not like this. Finally, you're referring to the sister board impedance, but I hope you did not just measure with a multimeter and make this assumption. Most circuits are non-linear with their supply demand, and it is not possible to measure the resistance and base the power supply decision around that.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago

    Hi Bin,

     

    The calculation is not right, you can use this web page to do it (the formula is there too):

    Voltage Divider Calculator

    However, unless your sister board has very low current requirement (much less than the current through the resistors - you can type in the resistor value and the voltage at this page to find out the current, or just use Current=Voltage/Resistance : Ohms Law Calculator ) then the answer is you'll need something else, most likely a DC-DC converter. If you provide more information about the sister board, then it is possible to help more. Similarly, although you have not specified the base board (which makes it harder to help you again), it sounds like a computer power supply. If you are not going to use the other two outputs, then please confirm it will operate if you do not use the other two outputs at all because some older computer PSUs may not like this. Finally, you're referring to the sister board impedance, but I hope you did not just measure with a multimeter and make this assumption. Most circuits are non-linear with their supply demand, and it is not possible to measure the resistance and base the power supply decision around that.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • houandreas
    0 houandreas over 8 years ago in reply to shabaz

    thx for the answer, im using the sp601 evaluation board. I will try a converter first.