Power & Energy
  • Technologies
  • More
Power & Energy
Forum converting to 5V power supply
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 3 answers
  • Subscribers 283 subscribers
  • Views 1446 views
  • Users 0 members are here
Related

converting to 5V power supply

houandreas
houandreas over 8 years ago

Hi, I have a base board which offers 2.5V@8A, 3.3V@8A and 12V@1A power supply but my sister board need 5V. So I'm considering to convert 12V to 5V, can I just use two resistors (10k and 24k ohm) to do that? This is under assumption that the sister board's impedance is high so I'm not sure if this simple circuit works. It should work but I'm rly not sure.. first time for me doing this.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +6 suggested
    Hi Bin, The calculation is not right, you can use this web page to do it (the formula is there too): Voltage Divider Calculator However, unless your sister board has very low current requirement (much…
  • jw0752
    jw0752 over 8 years ago +5 verified
    Hi Bin, This little DC / DC converter will work well for your application. I have used them in similar applications. http://www.newark.com/recom-power/r-78e5-0-0-5/dc-dc-converter-2-5w-5v-0-5a-sip/dp/62X9499…
  • genebren
    genebren over 8 years ago +3 suggested
    Hi Bin, Both shabaz and jw0752 have offered some sound advice (as they are known to do around here). Another simple and perhaps lower cost approach might be a simple 5.0V regulator. This is feasible is…
  • shabaz
    0 shabaz over 8 years ago

    Hi Bin,

     

    The calculation is not right, you can use this web page to do it (the formula is there too):

    Voltage Divider Calculator

    However, unless your sister board has very low current requirement (much less than the current through the resistors - you can type in the resistor value and the voltage at this page to find out the current, or just use Current=Voltage/Resistance : Ohms Law Calculator ) then the answer is you'll need something else, most likely a DC-DC converter. If you provide more information about the sister board, then it is possible to help more. Similarly, although you have not specified the base board (which makes it harder to help you again), it sounds like a computer power supply. If you are not going to use the other two outputs, then please confirm it will operate if you do not use the other two outputs at all because some older computer PSUs may not like this. Finally, you're referring to the sister board impedance, but I hope you did not just measure with a multimeter and make this assumption. Most circuits are non-linear with their supply demand, and it is not possible to measure the resistance and base the power supply decision around that.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago

    Hi Bin,

     

    This little DC / DC converter will work well for your application. I have used them in similar applications.

     

    http://www.newark.com/recom-power/r-78e5-0-0-5/dc-dc-converter-2-5w-5v-0-5a-sip/dp/62X9499?st=Recom%20R

     

    It will give you up to 500 mA. If you need more current there is also a version that will deliver 1 Amp. shabaz  is correct, the resistors will not work properly and would not be stable or efficient.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago

    Hi Bin,

     

    Both shabaz and jw0752 have offered some sound advice (as they are known to do around here).  Another simple and perhaps lower cost approach might be a simple 5.0V regulator.  This is feasible is the supply currents are low enough that the regulator is not called upon to dissipate too much power (not a problem with the DC-to-DC convertors mentioned above).  As an example, if the load current is 100ma, the regulator would dissipate (12v-5v) * 0.1A, or 0.7Watts, which could fall outside of the parts specification.  As a side note, some DC-to-DC convertors can generate a lot of high frequency noise, that might cause other issues (on the main board and the sister board), so be aware, should you see any performance issues in your project.

     

    Good luck and welcome to the Element14 community!

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • houandreas
    0 houandreas over 8 years ago in reply to shabaz

    thx for the answer, im using the sp601 evaluation board. I will try a converter first.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • houandreas
    0 houandreas over 8 years ago in reply to genebren

    thx, i would try a converter first. I also had a look at the base board and found that it uses 3 regulators to offer these 3 kinds of power sources. The power it uses is also 5V and converted to 2.5V,3.3V,12V for user use. And as mentioned in question they support up to 8A,8A,1A, with the calculation you mentioned it can dissipate (5v-2.5v)*8A=20 Watts.Why isn't it a problem? If it's just the regulator's difference, is it ok for me to use one if pay attention to the regulators specification?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to houandreas

    Regulators can be build that will handle several watts.  In addition, heatsinks and good PCB layouts can extend the range by helping to dissipate heat into the air and/or other materials, so that the chip does not over heat.  There are also other techniques, like adding inline diodes to the regulator input to reduce the voltage drop across the regulator (5Vin-0.7Vd- 2.5Vout) * 8A = 14.4Watts (will offering reverse voltage protection).  These are all steps to finding and using regulators without damaging them.

    Good Luck with your project.

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • houandreas
    0 houandreas over 8 years ago in reply to genebren

    thx for your answerimage that sounds interesting

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    If you wanted to be really crude you could use a high-ish value resistor and a 5v zener to derive 12V.  It's a bit ugly but cheap and easy if you get the current calcs correct!