Power & Energy
  • Technologies
  • More
Power & Energy
Forum Dealing With Low Battery
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 8 answers
  • Subscribers 285 subscribers
  • Views 3303 views
  • Users 0 members are here
  • control
  • battery
  • power
  • solar
  • remote
  • sensor
Related

Dealing With Low Battery

ntewinkel
ntewinkel over 8 years ago

Hi All,

 

I'm hoping to use solar for powering micro controller data logging/sensing projects.

 

Specifically, I have an ESP-8266 (like Adafruit's Huzzah) based project I'd like to run on solar. (the temperature logger I blogged about recently)

 

The ESP, being WiFi enabled, uses a fair bit of power to communicate, and I would like to avoid any issues with brownout or shutdown at bad times. And also perhaps issues with startup/shutdown flickering.

 

The challenges include:

1. charging a battery from the solar panel.

2. output of the battery has to provide 3.3v to power the board

3. battery should be sufficiently charged before it provides power to the board

4. battery should shut down the board (cut the power) when voltage goes too low

5. The micro controller should be super energy efficient - ie, sleep most of the time, wake up just long enough to do something, then sleep again.

 

I'm still having trouble wrapping my mind around points 3 and 4.

 

Mark mcb1 suggested:

>For the Forget me Not challenge, the EnOcean devices reduced their reporting rate to suit the charge they had.

 

Which is a great idea - dynamically adjusting sleep and wake times depending on battery voltage. But I think it only addresses part (most) of the concerns.

 

My more direct concern with 3 and 4 was more outside of the control of the microcontroller: can we keep the battery controller from providing any power at all until a minimum threshold is achieved? ie, if battery pack voltage drops to the minimum 3.2volts, shut off power to the microcontroller, and then don't provide power again until it's back up to, say, 3.4 volts. I suppose a very power-miser type controller could control that part (digispark maybe?). So the battery would need enough power to run the digispark, and the digispark would turn on a relay if it figures there's enough power to run the ESP8266. I'm pretty sure I've seen battery protection circuits out there that will avoid over-discharge that can shut off power to the digispark in those cases.

 

I guess there's also that detail about not cutting power to the ESP when it's in the middle of communications.

 

Thanks,

-Nico

 

ps, This discussion started in another thread, but I thought it could use its own spot, mostly for future reference for all of us image

 

pps, The rough approach is to just set it up and hope it doesn't run out of power much, and else just let it deal with it, but I'm looking for a gentler more refined solution.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +5 suggested
    ntewinkel I ran across this post on the LowPowerLab site. https://lowpowerlab.com/2017/09/15/weathershield-supercapacitor-tiny-solar-cell/ Using a supercap might be an alternative. Mark
  • mcb1
    mcb1 over 8 years ago +4 verified
    Seems you need this https://www.adafruit.com/product/3428 A voltage detector is handy for projects where you want to make sure your microcontroller doesn't run at a low voltage. For example, say you have…
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft +4 suggested
    Hi Raymond, Thanks for that link. It looks like a more general 12volt kind of setup. I've done that before with bigger panels and a controller, charging a bank of 12v batteries. Unfortunately the panels…
Parents
  • ntewinkel
    0 ntewinkel over 8 years ago

    Further to the idea of using a Digispark as a power controller:

    http://digistump.com/wiki/digispark/quickref

     

    About halfway down the page is a sketch:

    "The following will display on the LCD the current voltage coming into the Digispark without having to use a pin to measure it!"

     

    Which opens up the possibility of using the Digispark (or any similar board like Adafruit Trinket, or even bare ATTiny85 chip) as a gate keeper:

    1. Modify the above mentioned sketch to monitor high and low power levels

    2. Listen for "active" signal from ESP board

    3. Super low level is monitored by hardware - ie, the battery protection circuit shuts off all power at a certain point.

    4. When Digispark starts up, relay (or transistor) is off so no power goes to the ESP board

    5. When Digispark detects voltage is above a safe level, it powers up the ESP board

    6. When ESP power is on, and Digispark detects voltage going below that safe level, it waits for "active" signal from ESP board to go low, and then shuts off power to the ESP board.

    7. Repeat back to step 5

     

    The assumption is of course that the ESP board is programmed to be a good citizen to not keep "active" high for extended periods of time.

     

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 8 years ago

    Further to the idea of using a Digispark as a power controller:

    http://digistump.com/wiki/digispark/quickref

     

    About halfway down the page is a sketch:

    "The following will display on the LCD the current voltage coming into the Digispark without having to use a pin to measure it!"

     

    Which opens up the possibility of using the Digispark (or any similar board like Adafruit Trinket, or even bare ATTiny85 chip) as a gate keeper:

    1. Modify the above mentioned sketch to monitor high and low power levels

    2. Listen for "active" signal from ESP board

    3. Super low level is monitored by hardware - ie, the battery protection circuit shuts off all power at a certain point.

    4. When Digispark starts up, relay (or transistor) is off so no power goes to the ESP board

    5. When Digispark detects voltage is above a safe level, it powers up the ESP board

    6. When ESP power is on, and Digispark detects voltage going below that safe level, it waits for "active" signal from ESP board to go low, and then shuts off power to the ESP board.

    7. Repeat back to step 5

     

    The assumption is of course that the ESP board is programmed to be a good citizen to not keep "active" high for extended periods of time.

     

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer