Power & Energy
  • Technologies
  • More
Power & Energy
Forum Any DC-DC adjustable regulator suggested to drive some LEDs
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 15 answers
  • Subscribers 285 subscribers
  • Views 2551 views
  • Users 0 members are here
  • LED driver
  • dc-dc regulator
  • multiple white led
Related

Any DC-DC adjustable regulator suggested to drive some LEDs

luislabmo
luislabmo over 7 years ago

Hello all,

 

I need a good adjustable DC-DC regulator suggestion. My main goal -for now- is to drive some LEDs in parallel, this is more or less what I'm looking for:

  • At least 600mA output with good efficiency (I think LDOs are not a good option here). I'm planning to drive 18 white LEDs (~3.2V, 30mA each), and of course if this can be used for other projects/applications that'd be ideal!
  • Adjustable: I need to tune the voltage a little down so the LEDs don't get too hot -adding a heat-sink is out of question- and as an added bonus this will reduce a little the power consumption
  • Very, very small package: I have very, very little room to work. This has to come in a very small package (SOT-23-5 or around that size) with very few parts required -and don't worry I can solder almost any SMD
  • Input Voltage: I want to power the thing with 3 or 4 rechargeable AA or AAA batteries (1.2V each).
  • US stock, around $2 each for few (maybe 4 or 5 of them) image

 

At first I came with the ON Semi NCP1529ON Semi NCP1529 (NCP1529 datasheet) which comes in a nice and small UDFN6 (2x2mm) but tbh, I'm kinda stuck in the part where I have to select the right Inductor (L1) and C2 (Cout) for my needs -too hard to digest-, below a simplified diagram of what I have:

image

 

Luis

  • Sign in to reply
  • Cancel

Top Replies

  • 14rhb
    14rhb over 7 years ago +4 suggested
    Hi Luis, Have you had a look at the Texas Instruments WebBench software? There are tools in that for selecting LED drivers based on your constraints. I'll try and get you some links. Rod
  • genebren
    genebren over 7 years ago +4 suggested
    Luis, I did not see your simplified diagram? This looks like a pretty good choice. I have worked with a few similar parts, and while I agree that component selection looks difficult, I have never needed…
  • Fred27
    Fred27 over 7 years ago in reply to 14rhb +4 suggested
    I'd also agree with 14rhb that you'd be better looking at an LED driver rather than just a DC/DC. You'll get better control of the current through the LEDs without losing loads of power in series resistors…
Parents
  • genebren
    0 genebren over 7 years ago

    Luis,

     

    I did not see your simplified diagram?

     

    This looks like a pretty good choice.  I have worked with a few similar parts, and while I agree that component selection looks difficult, I have never needed to move too far away (if at all) from the recommended or typical component values (2.2uH and 10uF).  If I can not find one of their recommended part numbers, I use the specification of one to search for a similar replacement part.  The might be a pretty tough package to solder (UDFN6), but if you feel comfortable with that, then sure the space saving would be nice.

     

    In a quick search, I found a similar part (AP3419, Diodes Inc.), which does not seem to be carried at Newark.  This uses very similar typical value components (2.2uH, maybe a little bigger Cout).

     

    Good luck with your design!

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • luislabmo
    0 luislabmo over 7 years ago in reply to genebren

    Thanks Gene,

     

    I will stick with your recommendations (typical component values) while on my design, hopefully it won't need many iterations.

     

    All the best,

     

    Luis

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • luislabmo
    0 luislabmo over 7 years ago in reply to genebren

    Thanks Gene,

     

    I will stick with your recommendations (typical component values) while on my design, hopefully it won't need many iterations.

     

    All the best,

     

    Luis

    • Cancel
    • Vote Up +4 Vote Down