Power & Energy
  • Technologies
  • More
Power & Energy
Forum Any DC-DC adjustable regulator suggested to drive some LEDs
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 15 answers
  • Subscribers 284 subscribers
  • Views 2572 views
  • Users 0 members are here
  • LED driver
  • dc-dc regulator
  • multiple white led
Related

Any DC-DC adjustable regulator suggested to drive some LEDs

luislabmo
luislabmo over 7 years ago

Hello all,

 

I need a good adjustable DC-DC regulator suggestion. My main goal -for now- is to drive some LEDs in parallel, this is more or less what I'm looking for:

  • At least 600mA output with good efficiency (I think LDOs are not a good option here). I'm planning to drive 18 white LEDs (~3.2V, 30mA each), and of course if this can be used for other projects/applications that'd be ideal!
  • Adjustable: I need to tune the voltage a little down so the LEDs don't get too hot -adding a heat-sink is out of question- and as an added bonus this will reduce a little the power consumption
  • Very, very small package: I have very, very little room to work. This has to come in a very small package (SOT-23-5 or around that size) with very few parts required -and don't worry I can solder almost any SMD
  • Input Voltage: I want to power the thing with 3 or 4 rechargeable AA or AAA batteries (1.2V each).
  • US stock, around $2 each for few (maybe 4 or 5 of them) image

 

At first I came with the ON Semi NCP1529ON Semi NCP1529 (NCP1529 datasheet) which comes in a nice and small UDFN6 (2x2mm) but tbh, I'm kinda stuck in the part where I have to select the right Inductor (L1) and C2 (Cout) for my needs -too hard to digest-, below a simplified diagram of what I have:

image

 

Luis

  • Sign in to reply
  • Cancel

Top Replies

  • 14rhb
    14rhb over 7 years ago +4 suggested
    Hi Luis, Have you had a look at the Texas Instruments WebBench software? There are tools in that for selecting LED drivers based on your constraints. I'll try and get you some links. Rod
  • genebren
    genebren over 7 years ago +4 suggested
    Luis, I did not see your simplified diagram? This looks like a pretty good choice. I have worked with a few similar parts, and while I agree that component selection looks difficult, I have never needed…
  • Fred27
    Fred27 over 7 years ago in reply to 14rhb +4 suggested
    I'd also agree with 14rhb that you'd be better looking at an LED driver rather than just a DC/DC. You'll get better control of the current through the LEDs without losing loads of power in series resistors…
Parents
  • shabaz
    0 shabaz over 7 years ago

    Hi Luis!

     

    I think it may be easier to go step-up, and drive a load of LEDs in series. TI has some parts that would provide around 40V, they are intended for backlighting (such as TFT panels). That's not a high enough voltage for 18 LEDs, so you could have (say) a couple of parallel chains of 9 series LEDs. That way, just a couple of resistors are needed, one per series chain.

    With the lower voltage all-parallel method, if there is no series resistor for each LED, unless all the LEDs come from the same batch, there will be brightness differences, it may not matter too much, but it could be noticeable. Modern LEDs seem to have less variation, but it could catch one out once these are being manufactured, so safer to have the resistors there to reduce this risk.

     

    EDIT: e.g. see LM2733, there is a table in the datasheet with component values for providing 30V at up to 110mA, that might just be enough to have two chains of 9 LEDs, or tweak the values for slightly higher than 30V.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Fred27
    0 Fred27 over 7 years ago in reply to shabaz

    I definitely think running them all in parallel is risky. There's a quick way to check though. I know Luis has a decent PSU as he sent me an adapter for the Keysight E36313A. (Thanks again, Luis!) Stick the LEDs in parallel, crank up the voltage slowly and see what happens. I suspect the LED with the lowest forward voltage drop will spoil the party and draw more current than the others. My guess would be at best uneven brightness and at worst that one LED blows.

     

    Two chains of 9 or three chains of 6 should make it easier. If you set the voltage to be just a little higher than the summed forward drops then you can get away with a low value series resistor and very little wasted power. Or maybe now an LED driver is feasible as you have only a few higher voltage chains to drive.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • luislabmo
    0 luislabmo over 7 years ago in reply to Fred27

    Hello David,

     

    I see where you are going image. I'm making sure to use LEDs with same part #/batch for my project, so in theory none should spoil the party. I see you love LED drivers , there is one catch with them, not good for driving LEDs in parallel; if for some reason one LED stops working, current will go up for the remaining working LEDs which may spoil the party. I may add a resistor in series to avoid problems but then I will go back to the "a LED driver physically too big and won't fit" problem or the thing may get too hot if such thing happens.image

     

    But, you and shabaz gave me a nice idea!. I might explore a step-up regulator and drive 2 or 3 chains in series with a resistor.

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Fred27
    0 Fred27 over 7 years ago in reply to luislabmo

    I'm only a fan of LED drivers (in this case) because they control the current rather than voltage for you. image Each output shouldn't be driving paralleled LEDs. Nothing should, whether it's a current or voltage source. Paralleled LEDs are never a good idea and that link you provided is exactly my point. It applies even more so to the voltage regulator you were proposing as to a current source like an LED driver.

     

    A step up regulator with LED chains definitely seem like the way to go. Kirchoff's law tells you the each LED in a chain has the same current and hence brightness. A small resistor should give you a good balance between power loss and sensitivity to the LED forward voltage drop.

     

    Don't forget to show us the suitably scary end result. image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • luislabmo
    0 luislabmo over 7 years ago in reply to Fred27

    Hello Fred27

     

    The "suitably scare end result" is complete!.

     

    Thank you ALL for all of your contributions.

     

    Luis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • luislabmo
    0 luislabmo over 7 years ago in reply to Fred27

    Hello Fred27

     

    The "suitably scare end result" is complete!.

     

    Thank you ALL for all of your contributions.

     

    Luis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer