Power & Energy
  • Technologies
  • More
Power & Energy
Forum NiMH battery pack charger
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 3 answers
  • Subscribers 284 subscribers
  • Views 1192 views
  • Users 0 members are here
  • battery controllers
  • nicd/nimh_battery_charger
Related

NiMH battery pack charger

koudelad
koudelad over 7 years ago

Hello,

 

About 10 years ago, all the major semiconductor manufacturers offered IC for battery management. Now looking at Texas Instruments, Maxim, Microchip and can't find a single device for charging a pack of 6 NiMH cells (industrial AAA cells) - 7.2 V, 600 - 750 mAh. The packs have an integrated NTC for temperature monitoring.

 

I have two use cases:

1) just a charger that will be able to charge them within ca. 2 hours (0.5 - 1 C with correct charge detection).

2) charger that will be able to charge the batteries and power a target device (ca. 50 - 100 mA power consumption) - that would be OK with a slow 0.1 C (a even a bit less). The slow charging alone could be easily done via LM317 etc. in constant current mode, but I have no idea how to handle the power consumption of the target device.

 

Any ideas? I would prefer either some relatively simple solution like LM317 or some specialized charger IC, but preferably with some ready-made evaluation board available.

 

Thank you,

David

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 7 years ago +4 suggested
    You could try the MAX713 as well - https://www.maximintegrated.com/en/products/power/battery-management/MAX713.html - Gough
  • shabaz
    shabaz over 7 years ago +3 verified
    Hi David, I think it could be worth making one from scratch in that situation : ( As you say, the charger IC options are limited. Since it has integrated NTC, that's a nice way to (fairly) quickly detect…
  • luislabmo
    luislabmo over 7 years ago +3 suggested
    Have you explored the Maxim DS2715BZ+ Maxim DS2715BZ+ ?. It can handle up to 10 NiMH batteries and has FAST-CHARGE up to 2C, monitors voltage, temperature and time. In the datasheet there are couple of…
Parents
  • koudelad
    0 koudelad over 7 years ago

    Thank you all for the replies.

     

    I overlooked the Maxim portfolio when looking at their website. It is clear that all the "classic" chargers  like MAX713 are slowly becoming not recommended for new designs, as the electronic devices are moving away from NiMH packs.

    The parts are available, but not the development kits, which just confirms that.

     

    There seems to be a portfolio of universal multi chemistry chargers, which basically incorporate a micro-controller.

     

    I am grateful for the ideas, I will take a few days to think it over and decide, which way to go.

     

    David

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • koudelad
    0 koudelad over 7 years ago in reply to koudelad

    And thanks shabaz for mentioning the ideal diode circuit, I haven't heard of it yet.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • koudelad
    0 koudelad over 7 years ago in reply to koudelad

    And thanks shabaz for mentioning the ideal diode circuit, I haven't heard of it yet.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer