Power & Energy
  • Technologies
  • More
Power & Energy
Forum Where to get LEDs rated for 1 to 1.5v
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 12 answers
  • Subscribers 282 subscribers
  • Views 19472 views
  • Users 0 members are here
Related

Where to get LEDs rated for 1 to 1.5v

hafcanadian
hafcanadian over 8 years ago

I have tried to repair a solar flickering garden pagoda light.  Unlike all the other types of that device I own, this one uses one AA NiMh battery rather than two.  It’s LED needs replacing because one of its wires had broken where it entered the “glass” head.

 

I got some 5mm wide-angle straw hat (stubby length) yellow/amber LEDs from Lighthouse LEDs last year, but illness kept me away from the task until this week.  The replacements from Lighthouse are 2v, but I guess I’d assumed that was a maximum rating.  Unfortunately no, Lighthouse now informs me they need at least 2 volts to light up, which on reflection makes sense.  It explains why the new lamp I soldered in wouldn’t light up... I initially thought I’d ruined the lamp with solder heat, and soldered in another using multiple heat sinks.  It didn’t light either.  Then I touched leads from a fresh AA battery to a lamp fresh out of the shipping bag, and it wouldn’t light.  Ah ha moment... dumb me.  My assumption that 2v was a max, because it was the lowest voltage lamp I could find, was ill advised.  But being an LED neophyte I seem always ignorant of their technics, as numerous faulty Xmas LED strings lying comfoundingly unrepaired in a bag will attest.

 

I think the circuit board controls the flame-like flickering because the original lamp was a straw hat.  But just in case, I also got from Lighthouse some standard 5mm self-flicker lamps at the same time.  What I can’t figure out is how the original LED worked on a single AA battery.  Lighthouse says I shouldn’t need a resistor in the circuit, but there is a coded red-green-red-silver one on the board.  Perhaps that is to control the current coming in during midday from the solar panel?  Regardless, surely the original LED must be a 1 volt lamp?  But where can I purchase such an animal?  Lighthouse claims to not be aware of any such device.

 

I guess I could try adding a second AA NiMh battery to bump the unit to 3v, but the box is only big enough for one and I don’t know but what the diodes and other CB components may not play well with 3 volts, nor if the panel has enough output potential to fully charge two NiMh AAs, even if they were only 600mAh ones.

 

Thanks in advance for any thoughts,

Joel

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +7 verified
    Joel, There are not many (if any) visible spectrum LEDs that will run directly from a single AA battery. But, most of the inexpensive solar/LED devices, using a single AA battery use a device (like cx2601…
  • jw0752
    jw0752 over 8 years ago +7 suggested
    Hi Joel, I was set up to do some experiments this evening and so I decided to take apart a cheap dollar store outside LED light and check the voltages. I knew that they operate on one 1.25 volt NiMH battery…
  • hafcanadian
    hafcanadian over 8 years ago +7 suggested
    Thanks to all who’ve responded. The idea of an inductor that boosts voltage makes a great deal of sense. I can see where the AA battery would not work directly, and my suspicions that the 2v rating for…
Parents
  • hafcanadian
    0 hafcanadian over 8 years ago

    Thanks to all who’ve responded.  The idea of an inductor that boosts voltage makes a great deal of sense.  I can see where the AA battery would not work directly, and my suspicions that the 2v rating for the LED means just that and is not a “max” is confirmed.  In my relatively simple mind I envision the inductor building voltage through resistance in a nanosecond, releasing it at 2 volts that activates the LED emission, and repeating the cycle producing the effect of the candle flicker.  The self-flickering LEDs I “just-in-case” bought shouldn’t be necessary.

     

    I am aware of the polarity for the LED wires and was careful to correctly solder the black and white leads to them.  My biggest inhibitor is my essential tremor.  If you don’t have that malady yet, pray that you never do.  It makes it exceedingly difficult to hold a soldering iron, solder, and wires steady enough to get a clean result anymore.  I try using normally spring-closed tweezers and other heat sink devices to hold parts together, and brace my hands on things, and when workable an alligator clip/magnifier/wand holder stand, but it’s still a frustrating challenge.  So forgive any sloppy-appearing workmanship in the pix.

     

    It would appear that the green device I thought was just a plain but large resistor is more so the inductor “coil”.  Although it does have continuity across it, perhaps it’s not working to boost the voltage as intended.  Or as you’ve suggested, one of the other components is faulty.  There’s only 2 diodes, a 4-pronged transistor (I think), and whatever the flat round brown component is.  The diodes have continuity in one direction okay, so I reckon it could be the transistor, which if what I’ve read is correct may be involved in the boost function?  I’ll also use my Optivisor headband magnifier to more closely examine the board for a micro-cracked or slopped solder point.

     

    As per Gene’s idea and cx2601 reference, I checked this article:  1.5 VOLT WHITE AND UV LED DRIVE CIRCUIT   .

    Its over my head in a lot of ways, but does offer insight that I can appreciate.  Shabaz, Douglas, and Gough... all your input has also been enlightening, so I now understand a lot more than I did.  It may come in handy in dealing with the other solar garden lanterns of various kinds in the future... a year doesn’t go by without at least one of them going belly up for some reason like corrosion, old batteries, spiders, or needing a new solar panel.  Some flicker (the best ones) and some don’t.  And to John, who helped this past week on another frustrating electrical repair project, another big thank you for the time and expertise you’ve contributed.

     

    I can take a couple more closeup pix of the cboard if anyone would like, appreciating any more analysis.  They are the simplest and most inexpensive lanterns we have and I’ve been tempted to just chuck them, but their effect at night is the most realistic of all.  It’s just that they have a history of not coming on in the evening after a day or two, which was frustrating, and why I tried disassembling one last year.  I suspect the panel in full sun all day isn’t enough, despite needing to charge only one battery (all our others use two).  Cheap lanterns or not, my curiosity and determination to learn and repair stuff perhaps has the better of me.

     

    Joel

     

    addendum:

    Okay, I always thought a capacitor was barrel shaped.  Apparently the brown disk shaped component I referred to in a paragraph above is known as a disc capacitor.  I see them in most circuit boards, but didn’t know what they were.  I’ve known “barrel” capacitors to fail, so why not this disk version, esp. if it’s supposed to store the built up voltage, and isn’t.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • hafcanadian
    0 hafcanadian over 8 years ago

    Thanks to all who’ve responded.  The idea of an inductor that boosts voltage makes a great deal of sense.  I can see where the AA battery would not work directly, and my suspicions that the 2v rating for the LED means just that and is not a “max” is confirmed.  In my relatively simple mind I envision the inductor building voltage through resistance in a nanosecond, releasing it at 2 volts that activates the LED emission, and repeating the cycle producing the effect of the candle flicker.  The self-flickering LEDs I “just-in-case” bought shouldn’t be necessary.

     

    I am aware of the polarity for the LED wires and was careful to correctly solder the black and white leads to them.  My biggest inhibitor is my essential tremor.  If you don’t have that malady yet, pray that you never do.  It makes it exceedingly difficult to hold a soldering iron, solder, and wires steady enough to get a clean result anymore.  I try using normally spring-closed tweezers and other heat sink devices to hold parts together, and brace my hands on things, and when workable an alligator clip/magnifier/wand holder stand, but it’s still a frustrating challenge.  So forgive any sloppy-appearing workmanship in the pix.

     

    It would appear that the green device I thought was just a plain but large resistor is more so the inductor “coil”.  Although it does have continuity across it, perhaps it’s not working to boost the voltage as intended.  Or as you’ve suggested, one of the other components is faulty.  There’s only 2 diodes, a 4-pronged transistor (I think), and whatever the flat round brown component is.  The diodes have continuity in one direction okay, so I reckon it could be the transistor, which if what I’ve read is correct may be involved in the boost function?  I’ll also use my Optivisor headband magnifier to more closely examine the board for a micro-cracked or slopped solder point.

     

    As per Gene’s idea and cx2601 reference, I checked this article:  1.5 VOLT WHITE AND UV LED DRIVE CIRCUIT   .

    Its over my head in a lot of ways, but does offer insight that I can appreciate.  Shabaz, Douglas, and Gough... all your input has also been enlightening, so I now understand a lot more than I did.  It may come in handy in dealing with the other solar garden lanterns of various kinds in the future... a year doesn’t go by without at least one of them going belly up for some reason like corrosion, old batteries, spiders, or needing a new solar panel.  Some flicker (the best ones) and some don’t.  And to John, who helped this past week on another frustrating electrical repair project, another big thank you for the time and expertise you’ve contributed.

     

    I can take a couple more closeup pix of the cboard if anyone would like, appreciating any more analysis.  They are the simplest and most inexpensive lanterns we have and I’ve been tempted to just chuck them, but their effect at night is the most realistic of all.  It’s just that they have a history of not coming on in the evening after a day or two, which was frustrating, and why I tried disassembling one last year.  I suspect the panel in full sun all day isn’t enough, despite needing to charge only one battery (all our others use two).  Cheap lanterns or not, my curiosity and determination to learn and repair stuff perhaps has the better of me.

     

    Joel

     

    addendum:

    Okay, I always thought a capacitor was barrel shaped.  Apparently the brown disk shaped component I referred to in a paragraph above is known as a disc capacitor.  I see them in most circuit boards, but didn’t know what they were.  I’ve known “barrel” capacitors to fail, so why not this disk version, esp. if it’s supposed to store the built up voltage, and isn’t.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Gough Lui
    0 Gough Lui over 8 years ago in reply to hafcanadian

    Disk capacitors are generally ceramic type, owing to its material nature, it's almost like a solid layer of ceramic with conductive metal layer deposited on the ceramic dielectric to form the capacitor. The assembly is then dipped in some protective paint/coating. It's a simple construction that lends itself to fairly reliable low-capacitance value capacitors, although if moisture gets in, the conductive metal layers could (in theory) oxidise and stop acting properly as an electrode, with consequent reduction in capacitance value.

     

    The round "barrel" type is likely to be an aluminium electrolytic capacitor. These are generally much larger value capacitors formed by "rolling up" electrodes soaked in electrolyte, insulated with plastic film. This assembly has much larger area resulting in higher capacitance, which is then shoved into a metal can with a sealing rubber bung from which your two terminals protrude (for the radial type, anyhow). These capacitors typically get used in power supplies and often fail because of a number of reasons - namely that they deal with high amounts of ripple in power supplies (a stressful application), that they (like every non-ideal capacitor) have an equivalent series resistance (ESR), that the ripple current through the ESR causes the capacitor to heat up, and that the electrolytic capacitors are sensitive to heat as this causes the rate of evaporation of the electrolyte to increase which also increases the ESR (which forms a runaway feedback loop) to my knowledge. As a result, these capacitors often "cook" and blow their vents (low-quality electrolyte formulation doesn't help) or they end up drying out (sometimes due to poor seals around the rubber bung) which reduces their capacitance to non-useful levels.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to hafcanadian

    Joel,

     

    I am not sure that the pattern that John captured on his scope will explain the flicker LED effect.  It is possible that his solar LED has a different chip than yours, but the pattern shown appears to be oscillating at a fixed pattern which is well above the eyes ability to see.  It is oscillation pattern is likely only used to boost the voltage.  Having said that, it would be possible to design a chip that modulated the switching pattern of the boost circuit to create a varying intensity on the LED (I just did not see any evidence of that in the switching rate of John's LED).

     

    Issues that might be effecting your LED lanterns:

     

    1) The batteries might not be able to hold a charge (or charge in the circuit).  Try another battery, or an external power source.  (Note: this simple devices do not follow manufactures specifications for battery charging.  They simply act as a simple trickle charger.  This may not allow the batteries to deliver the full charge available. They do not limit charge or protect against over voltage)

     

    2) Along the line of the batteries, but there may be corrosion on the battery terminals that is causing a poor connection.  Clean the battery connections.

     

    3) The solar panel may not be functional.  Try a fully charged battery.

     

    4) The LED that you have used may have higher forward voltage than the circuit is designed to provide.  In the lower current range of LEDs (<100mA), about 60% of those are rated below 3.5V.  Have you tried to illuminate the LED with a power supply or multiple batteries (with a current limiting resistor) to see what the turn-on voltage is?

     

    There could be other issues that are more difficult to diagnose (or guess) without further information.

     

    Good luck in getting these lamps to light.

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer