Power & Energy
  • Technologies
  • More
Power & Energy
Forum Looking for a specific type of pot/variable resistor
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 11 answers
  • Subscribers 288 subscribers
  • Views 2686 views
  • Users 0 members are here
  • rheostat
  • potentiometer
  • rotary
  • pot
  • variable resistor
  • resistor
Related

Looking for a specific type of pot/variable resistor

damonjohn20
damonjohn20 over 6 years ago

Hi,

 

I'm new to this site so I may be posting this question in the wrong location. I'm looking for a specific type of variable resistor, in my research I haven't been able to discover something that fits this description (probably due to my lack of industry knowledge and associated vocabulary). Considering that a regular 3 pin 10k pot has one common pin (pin 2) and 2 'output' pins (pins 1 and 3), the resistance between pins 1 and 2 + the resistance between pins 2 and 3 will always add up to 10k. I'm looking for something similar, but with 4 or 5 output pins, while still keeping the singular common pin. I drew a very crude diagram of the general idea of what I'm looking for. image

 

In the center of the semi-circle, this represents my common pin (preferably on a rotary) that adjusts the voltage across 4 output terminals.

 

If anyone knows the name of this type of component, I could figure out where to start in my research for the right one.

 

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago in reply to damonjohn20 +5 suggested
    Hi Damon, As promised I have used the special potentiometer that I found to prove that your idea for a potentiometer that can turn on different banks of LEDs as it is rotated is a viable idea. In this…
  • jw0752
    jw0752 over 6 years ago in reply to damonjohn20 +4 suggested
    Most potentiometers are not designed to handle power. You might get by with one or two LEDs but as soon as you try to handle more than this the pot will over heat and burn up. What you are describing will…
  • jw0752
    jw0752 over 6 years ago +3 suggested
    Hi Again Damon, For the fun of it I checked my stock and found this curiosity: This is a 3 gang potentiometer with one independent 1 meg gang at the front and two mechanically locked 425K gangs at the…
Parents
  • jw0752
    0 jw0752 over 6 years ago

    Hi Again Damon,

     

    For the fun of it I checked my stock and found this curiosity:

     

      imageimage

     

    This is a 3 gang potentiometer with one independent 1 meg gang at the front and two mechanically locked 425K gangs at the back. Each of the 425K gangs has a tap at 150K from each end with a net 125K  between the taps. If you happen to need one potentiometer like this one I will give you my address. If you need more than one you are out of luck as I probably salvaged it 40 years ago from an old TV and it is the only one like it that I have seen.

     

    I am really curious what type of circuit would need a control like this.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • damonjohn20
    0 damonjohn20 over 6 years ago in reply to jw0752

    In response to John and Luis both (not sure how to respond to both at once)

     

    Thanks for all your input, I have definitely worked with microcontrollers before, but was looking to simplify the schematic by avoiding the logical processing all together. Unfortunately I don't have the knowledge or experience (yet) to know the solutions that are or aren't available, hence this post!

     

    Based on all of this, it's definitely looking like I'm going to have to go with the microcontroller route. Your find of that unique pot is very interesting, I've definitely never been aware of any product that has a dual function rotary pot such as that one.

     

    Luis nailed it in saying that my pot concept wouldn't have touched on every RGB color combination possible. Assuming I was working with a single low power LED, I'd be interested to see if some combination of a pot like I drew and a few 10k resistors across the output pins could provide a desired result.

     

    Thanks again

     

    Damon

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to damonjohn20

    Tonight for the fun of it I will breadboard up a circuit to do what you describe, using the odd potentiometer that I have. We will see how it works out.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 6 years ago in reply to damonjohn20

    Tonight for the fun of it I will breadboard up a circuit to do what you describe, using the odd potentiometer that I have. We will see how it works out.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer