Power & Energy
  • Technologies
  • More
Power & Energy
Forum Peltier or Ground source heat pump (thermosyphon or heat pump)?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 284 subscribers
  • Views 993 views
  • Users 0 members are here
Related

Peltier or Ground source heat pump (thermosyphon or heat pump)?

ewkm
ewkm over 7 years ago

I am trying to devise am energy efficient way to cool a small  outdoor pond (approx 3 m  long by .3 m wide). I keep Axolotls in it and their optimum temperature is 60-64 F (16-18 C).  The pond is mostly under plant shade so it is more about the ambient air temperature being too high in summer (Western Australia - gets up to 45C).  I am, thinking either Peltier modules with solar panels to provide power, or thermosyphon  / heat pipe.

 

This is not a solar pond so the temperature differential between layers of water would not be so great. I am wanting to draw heat from the water into the warmer air above the pond.  

 

Any thoughts on the above or any other method you can think of would be appreciated. Not too keen on running a refrigerated setup as power consumption would be high.

 

cheers

 

Evan

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 7 years ago +3 suggested
    Hi Evan, The most efficient way to cool the pond would be for you to bury a hose several feet below the ground and circulate the pond water through it and let the earth pull the heat out of the water.…
  • dougw
    dougw over 7 years ago +2 suggested
    If you have extra water, using the latent heat of evaporation can extract a lot of heat. Simply blowing air across the water will increase evaporation and provide extra cooling. I think every liter of…
  • ewkm
    ewkm over 7 years ago in reply to dougw +2
    Excellent idea. Can run that off solar panel. My concern is whether the opposite of wind chill may occur on very hot days – i.e. blowing hot air over the water may increase the temperature. I guess it…
Parents
  • dougw
    0 dougw over 7 years ago

    If you have extra water, using the latent heat of evaporation can extract a lot of heat. Simply blowing air across the water will increase evaporation and provide extra cooling. I think every liter of water that evaporates extracts something like 541 kilocalories of heat. Every calorie decreases the temperature of 1 ml of water by 1 degree C.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ewkm
    0 ewkm over 7 years ago in reply to dougw

    Excellent idea. Can run that off solar panel.  My concern is whether the opposite of wind chill may occur on very hot days – i.e. blowing hot air over the water may increase the temperature.  I guess it will increase the evaporation rate and that would compensate. Be interesting to see.  Thank you.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ewkm
    0 ewkm over 7 years ago in reply to dougw

    Excellent idea. Can run that off solar panel.  My concern is whether the opposite of wind chill may occur on very hot days – i.e. blowing hot air over the water may increase the temperature.  I guess it will increase the evaporation rate and that would compensate. Be interesting to see.  Thank you.