Power & Energy
  • Technologies
  • More
Power & Energy
Forum Uninterrupted Supply With Lipo Battery
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 8 answers
  • Subscribers 284 subscribers
  • Views 3273 views
  • Users 0 members are here
Related

Uninterrupted Supply With Lipo Battery

alegassey
alegassey over 6 years ago

Hi,

   I've been trying to come up with a solution for a small project I am working on.  What I want to do is have two batteries, both Lipo because I need the current density.  One will be small and the other large.  The intended operation is to have the small battery as a backup while changing out the larger battery for a fully charged one.  Both batteries are single cell and they will feed into a 2.5V regulator for system power.  I have tried a few circuits with pfet and pnp BJT but I found that when the batteries have slightly different voltages I start drawing from the smaller battery when I don't want to.

 

Basically I am wondering if anyone knows of a circuit for UPS (uninterrupted power supply) or any off the shelf IC's that I can use to accomplish this task.

 

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +4 suggested
    Hi Allen, I am old so I tend to think more mechanical. For simplicity I would use a Make before break DPDT switch that could switch between the Main and Backup battery. That way you would only have to…
  • genebren
    genebren over 6 years ago +4 suggested
    Hi Allen, I have typically used Schottky didoes (low forward voltage drop) to steer either the battery voltage or the charging voltage into the voltage regulator. That way, when charging the battery, the…
  • alegassey
    alegassey over 6 years ago in reply to shabaz +4 suggested
    Thanks for the response and yes things got complicated quickly. I originally thought I had a solution working but since I was using a power supply I didn’t see the problem. Originally I intended to use…
Parents
  • jw0752
    0 jw0752 over 6 years ago

    Hi Allen,

     

    I am old so I tend to think more mechanical. For simplicity I would use a Make before break DPDT switch that could switch between the Main and Backup battery. That way you would only have to switch to backup while you replace the main battery and then switch back after the replacement is made. Likewise when the switch is on Main the backup battery could be replaced. The Make before break switch would have both batteries in parallel for a brief instant while the switch is passing from one position to the other. If you did not want to use a make before break switch I suspect that a Capacitor could be used to bridge the milli second while a standard DPDT switch transitioned.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • alegassey
    0 alegassey over 6 years ago in reply to jw0752

    I like the idea, but I’m really trying to make this automatic, with no need to throw a switch.

     

    Allen

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • alegassey
    0 alegassey over 6 years ago in reply to jw0752

    I like the idea, but I’m really trying to make this automatic, with no need to throw a switch.

     

    Allen

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer