Power & Energy
  • Technologies
  • More
Power & Energy
Forum Uninterrupted Supply With Lipo Battery
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 8 answers
  • Subscribers 284 subscribers
  • Views 3274 views
  • Users 0 members are here
Related

Uninterrupted Supply With Lipo Battery

alegassey
alegassey over 6 years ago

Hi,

   I've been trying to come up with a solution for a small project I am working on.  What I want to do is have two batteries, both Lipo because I need the current density.  One will be small and the other large.  The intended operation is to have the small battery as a backup while changing out the larger battery for a fully charged one.  Both batteries are single cell and they will feed into a 2.5V regulator for system power.  I have tried a few circuits with pfet and pnp BJT but I found that when the batteries have slightly different voltages I start drawing from the smaller battery when I don't want to.

 

Basically I am wondering if anyone knows of a circuit for UPS (uninterrupted power supply) or any off the shelf IC's that I can use to accomplish this task.

 

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +4 suggested
    Hi Allen, I am old so I tend to think more mechanical. For simplicity I would use a Make before break DPDT switch that could switch between the Main and Backup battery. That way you would only have to…
  • genebren
    genebren over 6 years ago +4 suggested
    Hi Allen, I have typically used Schottky didoes (low forward voltage drop) to steer either the battery voltage or the charging voltage into the voltage regulator. That way, when charging the battery, the…
  • alegassey
    alegassey over 6 years ago in reply to shabaz +4 suggested
    Thanks for the response and yes things got complicated quickly. I originally thought I had a solution working but since I was using a power supply I didn’t see the problem. Originally I intended to use…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi Allen,

     

    You just need the primary supply (the larger battery) to hold off the secondary supply, until there is absence of the primary supply.

    There are ICs that do this (see Linear Tech), look for 'ideal diode' and 'power supply OR'ing circuits' but if your requirements are very well defined (e.g. if you know precisely what the span of voltage will be for the primary and secondary sources) you could probably put something together with MOSFETs, or MOSFETs and diodes if you don't mind the volt drop. A more general purpose solution will use the ICs as mentioned above, but even they will have some restrictions based on the encountered voltages for the primary and secondary supplies.

    As you say, things get complicated fast if the voltages change, and there's no single simple solution.

    Depending on how much effort you want to put into solving the problem, you could even use comparators and some logic, or even use part of a microcontroller if you've already got one in your design.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • alegassey
    0 alegassey over 6 years ago in reply to shabaz

    I have actually ordered some ORing ics yesterday, waiting for them to come in, I will take a look at what you have suggested above,

     

    Thanks for taking the time to look at this.

         Allen

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • alegassey
    0 alegassey over 6 years ago in reply to shabaz

    I have actually ordered some ORing ics yesterday, waiting for them to come in, I will take a look at what you have suggested above,

     

    Thanks for taking the time to look at this.

         Allen

    • Cancel
    • Vote Up +3 Vote Down