Power & Energy
  • Technologies
  • More
Power & Energy
Forum Design of a low voltage and high current DC-DC converter
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 3 answers
  • Subscribers 284 subscribers
  • Views 5752 views
  • Users 0 members are here
  • dc-dc converters
Related

Design of a low voltage and high current DC-DC converter

s1m0n3t
s1m0n3t over 6 years ago

Hi all,

I'm dealing with a quite strange design. I have a single 5V power source with few amps of current (about 3A) and I need to drive a load (about 0.8mOhm of resistance, but variable in function of voltage/current) with a current from -10A to 10A, at 100mV of maximum voltage.

I'm searching for an IC which can help me, but I don't found any suitable device, at this moment.

I would try a discrete configuration like the following schematic:

image

I can send an alternate (square wave) current with one or another direction in the transformer, using a PWM signal on CTRL1 or CTRL2, with 50% duty cycle.

If i use a 10:1 ratio transformer (for example), I will have a reduced maximum voltage, but with more current (about 10 times). Correct?

And then, with another PWM on CTRL3 or CTRL4, I can modulate the output from zero to positive maximum and to negative minimum voltage, measuring the voltage to the feedback point, or the current in series of the load (R1) with an hall effect sensor.

I probably don't even need two input windings, but I can send a single square wave in input and activate Q3 or Q4 to obtain a positive or negative output. And perhaps one of the two outgoing mosfets should be type P?

What do you think about this solution? Anyone have alternative ideas or suggestions?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago +1
    Is the 100 mV a maximum, or a constant desired voltage? edit: reading the post again and the schematic, it looks like you want a swinging or switcheable output voltage between -100 and +100 mV? There's…
  • s1m0n3t
    s1m0n3t over 6 years ago in reply to Jan Cumps +1
    100mV is only a maximum, I need to regulate the current, so the voltage will depend on the load.
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to s1m0n3t +1 suggested
    Can I summarise it like this? - you need a device that can control a DC current between -10 A and + 10 A. That current has to be configurable and maintained by the circuit. - it's derived from the load…
Parents
  • michaelkellett
    0 michaelkellett over 6 years ago

    How accurately must you control the voltage/current ?

    How much noise is acceptable on the output.

    What sort of signal will you drive the load with ? (AC, slowly varying DC etc)

     

    (Can you tell us what the load is ?)

     

    I'm thinking that the best bet would be a 5V to 1V switching converter and then a linear bridge type power amplifier.

     

    Alternatively you could re-purpose the LT1923 which is a switching Thermo electric cooler driver. Even if you don't use this chip it would be worth reading the data sheet and app note to get some background information.

     

    I've used this chip and it works quite well, (although it's very expensive).

     

    Since the power FETs and sense resistor are off chip you can tune it up for whatever you want.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • s1m0n3t
    0 s1m0n3t over 6 years ago in reply to michaelkellett

    I need to control the current with a resolution of 10mA, preferably 1mA.

    A little noise won't be a big deal.

    The load will be controlled by a slowly varying DC, with a maximum variation of 10A in 1s.

    The load is a solenoid.

    Thank you for the suggested LT1923, I'm reading the datasheet now.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • s1m0n3t
    0 s1m0n3t over 6 years ago in reply to michaelkellett

    I need to control the current with a resolution of 10mA, preferably 1mA.

    A little noise won't be a big deal.

    The load will be controlled by a slowly varying DC, with a maximum variation of 10A in 1s.

    The load is a solenoid.

    Thank you for the suggested LT1923, I'm reading the datasheet now.