Power & Energy
  • Technologies
  • More
Power & Energy
Forum Design of a low voltage and high current DC-DC converter
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 3 answers
  • Subscribers 284 subscribers
  • Views 5761 views
  • Users 0 members are here
  • dc-dc converters
Related

Design of a low voltage and high current DC-DC converter

s1m0n3t
s1m0n3t over 6 years ago

Hi all,

I'm dealing with a quite strange design. I have a single 5V power source with few amps of current (about 3A) and I need to drive a load (about 0.8mOhm of resistance, but variable in function of voltage/current) with a current from -10A to 10A, at 100mV of maximum voltage.

I'm searching for an IC which can help me, but I don't found any suitable device, at this moment.

I would try a discrete configuration like the following schematic:

image

I can send an alternate (square wave) current with one or another direction in the transformer, using a PWM signal on CTRL1 or CTRL2, with 50% duty cycle.

If i use a 10:1 ratio transformer (for example), I will have a reduced maximum voltage, but with more current (about 10 times). Correct?

And then, with another PWM on CTRL3 or CTRL4, I can modulate the output from zero to positive maximum and to negative minimum voltage, measuring the voltage to the feedback point, or the current in series of the load (R1) with an hall effect sensor.

I probably don't even need two input windings, but I can send a single square wave in input and activate Q3 or Q4 to obtain a positive or negative output. And perhaps one of the two outgoing mosfets should be type P?

What do you think about this solution? Anyone have alternative ideas or suggestions?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago +1
    Is the 100 mV a maximum, or a constant desired voltage? edit: reading the post again and the schematic, it looks like you want a swinging or switcheable output voltage between -100 and +100 mV? There's…
  • s1m0n3t
    s1m0n3t over 6 years ago in reply to Jan Cumps +1
    100mV is only a maximum, I need to regulate the current, so the voltage will depend on the load.
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to s1m0n3t +1 suggested
    Can I summarise it like this? - you need a device that can control a DC current between -10 A and + 10 A. That current has to be configurable and maintained by the circuit. - it's derived from the load…
Parents
  • kkazem
    0 kkazem over 6 years ago

    After reading all the posts, and as a professional power converter engineer, I make the following observations:

    1. If yous load is only 0.8 mOhms with +/-10A max, the load voltage would only be 8 mV maximum.

    2. There is no need for a bipolar output (plus and minus) as the load is an isolated coil, so you can have one circuit to step-down and control the 0 to 10A load, and another after that to change output polarity to the load. The polarity changer would require a 4-mosfet bridge.

    3. To get the 8 mV at 10A from 5V at 3A, you only need a buck converter rated at 10A output that can run off 5V. There are probably many off the shelf. At 10% pwm duty cycle, the dc output from your 5V input would be 0.5V at 30A (more than enough current).  And most buck converters won't control well below 5%to 10% duty cycle. But there is a solution which is to put a resistor in series with your load. Compute the resistor nominally as (0.5V - 0.08V)/10A = 50 mOhms at 5W or more.

    4. The LT1923 can be used, but you'll have a lot of design work to do. Instead of using a temperature sensor as an input, you'll use the sensed output current, which probably must be level-shifted to being a ground-referenced signal instead of a floating bridge signal. The current can be sensed with a 10 mOhm to 50 mOhm resistor used as a current shunt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kkazem
    0 kkazem over 6 years ago

    After reading all the posts, and as a professional power converter engineer, I make the following observations:

    1. If yous load is only 0.8 mOhms with +/-10A max, the load voltage would only be 8 mV maximum.

    2. There is no need for a bipolar output (plus and minus) as the load is an isolated coil, so you can have one circuit to step-down and control the 0 to 10A load, and another after that to change output polarity to the load. The polarity changer would require a 4-mosfet bridge.

    3. To get the 8 mV at 10A from 5V at 3A, you only need a buck converter rated at 10A output that can run off 5V. There are probably many off the shelf. At 10% pwm duty cycle, the dc output from your 5V input would be 0.5V at 30A (more than enough current).  And most buck converters won't control well below 5%to 10% duty cycle. But there is a solution which is to put a resistor in series with your load. Compute the resistor nominally as (0.5V - 0.08V)/10A = 50 mOhms at 5W or more.

    4. The LT1923 can be used, but you'll have a lot of design work to do. Instead of using a temperature sensor as an input, you'll use the sensed output current, which probably must be level-shifted to being a ground-referenced signal instead of a floating bridge signal. The current can be sensed with a 10 mOhm to 50 mOhm resistor used as a current shunt.