Power & Energy
  • Technologies
  • More
Power & Energy
Forum Smps sine wave
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 5 answers
  • Subscribers 282 subscribers
  • Views 2908 views
  • Users 0 members are here
Related

Smps sine wave

bigsexy
bigsexy over 6 years ago

As I further learn about the intricacies of electronics and do not have an adequate oscilloscope I have a question regarding SMPS. I know how regular old go to hell transformers work and require a sine wave switching to positive and negative voltages to create the magnetic field induced into the iron core and so forth. But does a sine wave have to go Into negative voltages to work? Let me elaborate a little because I tend to over complicate my thoughts.
Lets say I have a mosfet that I use as a switch to pulse a dc voltage on and off at a significant speed in the kHz range through a wire wrapped in a coil on a transformer core, would that be able to create a half sine wave and therefore be used to induce a voltage in a secondary winding?

I am wondering if in a smps if the electronics recreate the sine wave to go high and low instead of high and off?

If this is confusing speak to you let me know and I will try to draw something up on paper and photo it for the thread.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +3 suggested
    It's too big a subject to explain in an answer here ! I had a quick Google for some tutorial type stuff and found this that isn't too bad: https://www.electronics-tutorials.ws/power/switch-mode-power-supply…
  • jc2048
    jc2048 over 5 years ago in reply to michaelkellett +3 suggested
    This is the best thing I've ever read on the subject, but I'm not sure it qualifies as an 'introduction' [someone reading it would need some familiarity with Faraday and Ampere and be capable of simple…
  • jc2048
    jc2048 over 5 years ago +3 suggested
    The waveform doesn't have to be a sinewave. If you'd like to see the effect of different waveforms, here's a selection from a pattern generator driving an old mains transformer that I found in one of my…
Parents
  • jc2048
    0 jc2048 over 5 years ago

    The waveform doesn't have to be a sinewave. If you'd like to see the effect of different waveforms, here's a selection from a pattern generator driving an old mains transformer that I found in one of my junk boxes.

     

    image

     

    The primary is marked 240V and the secondary 12V 100mA (the secondary has a tap, so it's really 24V across both: ie a transformer ratio of 10:1). I'm driving it at approximately 100Hz.

     

    image

    image

    image

    image

    image

     

    The waveforms speak for themselves. Yellow trace is the input from the generator, blue trace is the output measured with a 10x probe with no other load.

     

    You can see from that that there's nothing particularly special about a sinewave. The transformer bandwidth is fairly limited with its laminated-steel core [probably below 100kHz], so sharp features of the waveforms will round off [not really noticeable at 100Hz], and you can see that the output winding 'rings' on very abrupt edges [that's resonance with capacitance from the winding and the probe], but other than that it transmits the waveform reasonably well.

     

    In the days of valve [vacuum tube] amplifiers, transformers were often used to match the output of the amplifier to the lower impedance of the loudspeaker.

     

    The last waveform isn't pure ac and would be very dodgy if it were your mains waveform [I should think it would run the core into saturation and cause damage]. I can get away with it with the generator because of all the resistance involved [the generator has a 50 Ohm in series with the output and the primary winding resistance is about 730 Ohms] and the much lower voltage, so there isn't the capability to get the current to the kind of levels that you would see cause problems.

     

    In the case of a switched winding, the reason you don't need to balance the waveform [time-integral of the voltage summing to zero over the cycle] is that if you let the winding go, the core corrects for itself by generating the opposing voltage. For that to happen, there needs to be a suitable path for the current to run and sufficient time. This is where it all starts to get complicated because there are many ways to drive windings and to effect the core 'reset', and also two fundamental ways to use a transformer in a switching circuit, forward and flyback, depending on whether the energy flows through or gets stored.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 5 years ago

    The waveform doesn't have to be a sinewave. If you'd like to see the effect of different waveforms, here's a selection from a pattern generator driving an old mains transformer that I found in one of my junk boxes.

     

    image

     

    The primary is marked 240V and the secondary 12V 100mA (the secondary has a tap, so it's really 24V across both: ie a transformer ratio of 10:1). I'm driving it at approximately 100Hz.

     

    image

    image

    image

    image

    image

     

    The waveforms speak for themselves. Yellow trace is the input from the generator, blue trace is the output measured with a 10x probe with no other load.

     

    You can see from that that there's nothing particularly special about a sinewave. The transformer bandwidth is fairly limited with its laminated-steel core [probably below 100kHz], so sharp features of the waveforms will round off [not really noticeable at 100Hz], and you can see that the output winding 'rings' on very abrupt edges [that's resonance with capacitance from the winding and the probe], but other than that it transmits the waveform reasonably well.

     

    In the days of valve [vacuum tube] amplifiers, transformers were often used to match the output of the amplifier to the lower impedance of the loudspeaker.

     

    The last waveform isn't pure ac and would be very dodgy if it were your mains waveform [I should think it would run the core into saturation and cause damage]. I can get away with it with the generator because of all the resistance involved [the generator has a 50 Ohm in series with the output and the primary winding resistance is about 730 Ohms] and the much lower voltage, so there isn't the capability to get the current to the kind of levels that you would see cause problems.

     

    In the case of a switched winding, the reason you don't need to balance the waveform [time-integral of the voltage summing to zero over the cycle] is that if you let the winding go, the core corrects for itself by generating the opposing voltage. For that to happen, there needs to be a suitable path for the current to run and sufficient time. This is where it all starts to get complicated because there are many ways to drive windings and to effect the core 'reset', and also two fundamental ways to use a transformer in a switching circuit, forward and flyback, depending on whether the energy flows through or gets stored.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer