Power & Energy
  • Technologies
  • More
Power & Energy
Forum Multi (wide) Voltage LED using LM317
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 285 subscribers
  • Views 2562 views
  • Users 0 members are here
  • current
  • regulator
  • constant
Related

Multi (wide) Voltage LED using LM317

Malcolm
Malcolm over 17 years ago
Just a thought, we know you can change a linear voltage regulator like the LM317 into a series constant current regulator by just adding one resistor (loads of application notes on Farnell Web site) but can it be done with the LM431 adjustable shunt regulator?
Anyone know?

 

Regs (regards not regulator)

Malcolm

  • Sign in to reply
  • Cancel
Parents
  • samplerman
    0 samplerman over 17 years ago

    HI The LM341 could be used, but on its own it can only sink 100mA so it may be better to stay with a resistor. If however the device is used with a series pass transistor then higher currents may be passed. The most efficient approach though would be to use a switching regulator chip as 85 to 90% efficiencies can be acheived.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • samplerman
    0 samplerman over 17 years ago

    HI The LM341 could be used, but on its own it can only sink 100mA so it may be better to stay with a resistor. If however the device is used with a series pass transistor then higher currents may be passed. The most efficient approach though would be to use a switching regulator chip as 85 to 90% efficiencies can be acheived.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer