Power & Energy
  • Technologies
  • More
Power & Energy
Forum Multi (wide) Voltage LED using LM317
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 285 subscribers
  • Views 2548 views
  • Users 0 members are here
  • current
  • regulator
  • constant
Related

Multi (wide) Voltage LED using LM317

Malcolm
Malcolm over 17 years ago
Just a thought, we know you can change a linear voltage regulator like the LM317 into a series constant current regulator by just adding one resistor (loads of application notes on Farnell Web site) but can it be done with the LM431 adjustable shunt regulator?
Anyone know?

 

Regs (regards not regulator)

Malcolm

  • Sign in to reply
  • Cancel
  • samplerman
    0 samplerman over 17 years ago

    HI The LM341 could be used, but on its own it can only sink 100mA so it may be better to stay with a resistor. If however the device is used with a series pass transistor then higher currents may be passed. The most efficient approach though would be to use a switching regulator chip as 85 to 90% efficiencies can be acheived.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Malcolm
    0 Malcolm over 17 years ago

    Ah so it can be used as a constant current source.

     

    Just one (or two points) The resistor is ok if the input voltage is constant, I wanted to a wide input voltage range with a constant brightness, hence the constant current feed.

     

    Now is it always more efficient to use a switching regulator (certainly not cheaper)? I read an article that asked that same question and the answer was not always. It seems that if the differential voltage is small then it may be more efficient to use a linear regulator.

     

    Regards

    Malc

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 17 years ago

    ,image

    This above picture is the typical application circuit of LM431, it shows us how to adjust VKA. If we replace R1 with LEDs, LEDs current will be adjusted by R2 and Vref. If  Vref and R2 is constant, LEDs current will be constant too

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kemmi
    0 kemmi over 17 years ago in reply to e14 Contributor

    Switching Regulator.JPG

    From  efficiency point, maybe only LM431 is not a good solution because input resistor will share more power dissipation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 17 years ago in reply to kemmi

    Good solution. But the circuit is too complex. Especially the chopper is hard to adjust.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Malcolm
    0 Malcolm over 17 years ago in reply to e14 Contributor

    Constant Current with one resistor.bmp

     

     

     

     

    This is the circuit I would normally use to generate a constant current of about 25mA. The input voltage is anything up to 37volts. The required resistor is calculated (roughly) by 1.2 volts divided by the current required. Eg 1.2V/.025A= about 47 ohms Resistor power is  Voltage squared/Resistance (eg 1.2*1.2/47ohms = 30mW)  OR  Current*Current*Resistance The power disipitation in the LM317 is of course the voltage drop across it multiplied by the current flowing through it (eg same current as going through your LED, "current through a series circuit is the same")

    NOTE:-47 ohm resistor used

    LM317 (small TO-92 packages)  http://uk.farnell.com/jsp/search/browse.jsp;jsessionid=BBVYM0BUEM3HMCQLCIPZK0Q?N=551&Ntk=gensearch_001|gensearch_001&Ntt=lm317|to-92&Ntx=&displaytext=&_requestid=163594

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kemmi
    0 kemmi over 17 years ago in reply to Malcolm

    your solution is only for small power LED driver.How about Power LED(350mA current or more ) for resistor will result in lower efficiency

     

    ???.JPG

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 17 years ago in reply to kemmi

    In fact, your solution is a series regulator with discrete parts. The transistor will consume power like the resistance does in my solution. I agree that my solution is suitable for low power led only. For high power led application, I'd like to choose Malcolm's LM317 solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Malcolm

          Hello!

    If a 24VAC power supply, can be solved with the LM317 and the MOSFET controller. The solution is to link http://www.sper.hr/eng/wld.htm.Works for years. No inductors. Effiency about 70%. It can be used 1..8 LED.                         
    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jason
    0 Jason over 16 years ago in reply to e14 Contributor

    I don't think using a series regulator (LDO or some discrete parts) is a good idear for hight power LED(typical 350mA). we can count the power dissipation as Pd=350mA*(V_in-V_led).if we use a Multi (wide) Voltage,V_in-V_led will very large,that means we need a high power dissipation component and more heat-sink and more cost but low efficiency.by the way ,how can we desgn for the constant current control,it's another cost.

    If we using switch regulator ,the issue above is not a problem.You will say what about the cost? infact,a switch regulator is expensive than LDO,but you can compare the total cost as the same function you need(CC control,dimming,open/short protect e.g.),what is the result you've got?image

    But in some special application we can use series regulator for power LED,like the fixed DC input.we can design the V_in-V_led very small for decrease Pd.maybe LM317 is a good choose image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>