Power & Energy
  • Technologies
  • More
Power & Energy
Forum Multi (wide) Voltage LED using LM317
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 285 subscribers
  • Views 2567 views
  • Users 0 members are here
  • current
  • regulator
  • constant
Related

Multi (wide) Voltage LED using LM317

Malcolm
Malcolm over 17 years ago
Just a thought, we know you can change a linear voltage regulator like the LM317 into a series constant current regulator by just adding one resistor (loads of application notes on Farnell Web site) but can it be done with the LM431 adjustable shunt regulator?
Anyone know?

 

Regs (regards not regulator)

Malcolm

  • Sign in to reply
  • Cancel
Parents
  • Malcolm
    0 Malcolm over 17 years ago

    Ah so it can be used as a constant current source.

     

    Just one (or two points) The resistor is ok if the input voltage is constant, I wanted to a wide input voltage range with a constant brightness, hence the constant current feed.

     

    Now is it always more efficient to use a switching regulator (certainly not cheaper)? I read an article that asked that same question and the answer was not always. It seems that if the differential voltage is small then it may be more efficient to use a linear regulator.

     

    Regards

    Malc

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Malcolm
    0 Malcolm over 17 years ago

    Ah so it can be used as a constant current source.

     

    Just one (or two points) The resistor is ok if the input voltage is constant, I wanted to a wide input voltage range with a constant brightness, hence the constant current feed.

     

    Now is it always more efficient to use a switching regulator (certainly not cheaper)? I read an article that asked that same question and the answer was not always. It seems that if the differential voltage is small then it may be more efficient to use a linear regulator.

     

    Regards

    Malc