Power & Energy
  • Technologies
  • More
Power & Energy
Forum 24V AC to 12V DC Adapter
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 282 subscribers
  • Views 781 views
  • Users 0 members are here
Related

24V AC to 12V DC Adapter

e14 Contributor
e14 Contributor over 16 years ago

Hi All,

 

Any Idea about 24VAC to 12V DC adapter available with FCC , CE certified??

 

I need 12V DC @ min 1.5A from 24VAC , Source is of 24VAC,50VA max.

 

I prefer adapter with CE, UL certified ..

 

Let me know if any body has Idea about it

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    Hi Rizwan,

     

    Rare to find this spec anyways,

     

    Please look at below link, which leads you for 2 choices,

     

    If from UK use below link

    http://uk.farnell.com/jsp/search/browse.jsp?N=1004239+5033483+5053979+5053977+567243+567419&No=0&getResults=true&appliedparametrics=true&locale=en_UK&catalogId=&prevNValues=1004239+5033483+5053979+5053977&originalQueryURL=/jsp/search/browse.jsp%3FN%3D1004239%26No%3D0%26getResults%3Dtrue%26appliedparametrics%3Dtrue%26locale%3Den_UK%26catalogId%3D

     

    If you are from India use below link

     

    http://in.farnell.com/jsp/search/browse.jsp?N=1002795+5038820+5061145+5061147+313141+313339&No=0&getResults=true&appliedparametrics=true&locale=en_IN&catalogId=&prevNValues=1002795+5038820+5061145+5061147&originalQueryURL=/jsp/search/browse.jsp%3FN%3D1002795%26No%3D0%26getResults%3Dtrue%26appliedparametrics%3Dtrue%26locale%3Den_IN%26catalogId%3D

     

     

    Part Number ::AD-12160(1.6A) or AD-12200BSDT (2A), Can check out if suits your needs as has been qualified product to industry standards.

     

    you can also look at Model VR1T of Altronix

     

    Hope this should solve your needs.

     

    Regards

    Mohammed Tanvir

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to e14 Contributor

    Thanks Tanvir..

     

    It was really helpful, However I beileve the consumption on 12V DC in our desing will be minimum 1.25A ..Do you relly suggest to use unregulated 12V supply for that ?

     

    I also do not have any idea about the internal power supply design of the device, which will get 12V direct from this source..So I am not sure if I plug unregulated power source to it then what will happen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to e14 Contributor

    Thanks Tanvir..

     

    It was really helpful, However I beileve the consumption on 12V DC in our desing will be minimum 1.25A ..Do you relly suggest to use unregulated 12V supply for that ?

     

    I also do not have any idea about the internal power supply design of the device, which will get 12V direct from this source..So I am not sure if I plug unregulated power source to it then what will happen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to e14 Contributor

    Hi Rizwan,

     

    The products suggested are regulated PS. with required current ratings, is the reason you get constant 12V o/p for your needs. Can you tell let me know what exactly (product) are you powering up ?

     

    Regards

    Tanvir

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to e14 Contributor

    Hi Tanveer,

     

    Please note that , we are planing to power up USB hub which has screw terminal for the power in pin. Acording to the catalog of the hub, it requires maximum 1.25A current at 12V. The DC input range is from 9-24V DC.

     

    The Power supply suggested are unregulated for DC O/P and regulated for the AC as per the data sheet of the source.

     

    The regulation factor of the source is, around 20% (Data sheet doesn't have the information, for what load it is calculated, I believ it must be for the full load that is 2A for the second option)..

     

    In this case, voltage at 2A can go down upto,

     

    .35 = 12 - x/12

    12x.35 = 12 -x

    4.2=12 -x

    x=7.8V

     

    So system Volatge can go down to 7.8V at 2A..So at 1.25A may be it can go down to , 9.3V.Which is however in the range but what will happen on using this source we can't say any thing wihtout knowing the internal power supply design of the HUB ....

     

    Apart from this, These sources are quite costly as well..Please let me know if you have any other idea regarding the requirement. May be we can remove the requirement of UL listed..