Power & Energy
  • Technologies
  • More
Power & Energy
Forum Inductive charger
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 285 subscribers
  • Views 1659 views
  • Users 0 members are here
Related

Inductive charger

e14 Contributor
e14 Contributor over 16 years ago

I'm going to design an inductive charger and I have a lot of open questions and don't really where to start. I know about the principle how it works. I need help with several things.

The idea is to get 5-7VDC out oin the secondary side, and something like 100mA would be nice.

 

First of all, what switching frequency is suitable concerning size and efficency of components, and also regarding type approval issues? I think electrical toothbrushes uses approx. 60 kHz so maybe that is a suitable frequency.

Secondly, does anyone know about a design example I can use for a start?

Does anyone have any suggestions for suitable inductors? Supplier, part number etc?

  • Sign in to reply
  • Cancel
Parents
  • enrico.migchels
    0 enrico.migchels over 16 years ago

    Hi there Roger,

     

    It seems that you are trying to re-invent the wheel :-) SMPS chargers (3-5W) are readily available on the market for just a few dollars. However if the task is related to 'having fun' this is something else. However if you don't have expierence in switch mode power supplies this task is not easy. Remember also that you are dealing with a device which has a safety function. (a user must be able to touch the output voltage safely). You as designer are responisible for this safety function. Given all this, your circuit should be a flyback converter. Getting a suitable (and safe) transformer is difficult, other components are easy to get.

     

    A switching frequency of 60kHz is not uncommon. Your power switch is a MOSFET and the controller is a small 8pin device from a supplier such as ST, ON, etc. If you look at the datasheet of such a controller (UC3842B is old but a generic part) you will find a typical application. You can downscale it for your needs.

     

    If you have specific questions i might be able to help you.

     

    Best regards and lot's of luck

     

    Enrico Migchels

    Power Conversion Design Engineer

    Heliox. B.V.

    Best, The Netherlands

    www.heliox.nl

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to enrico.migchels

    Hi Enrico!

     

    Thank you for your answer.

     

    I'm sorry, but I was maybe clera enough with my question:

     

    I have a lot of experience with power supply designs in general with for examples DC/DC converts with all kind of topologies.

    What I want to do now is something that is similar to an inductive charger for an electrical toothbrush, menaing with one part that act as a "transmitter" but that are completly sealed and not possible to touch any electrical parts.

    The second part shall act as a "receiver" (toothbrush) and is also completly sealed.

     

    So, I will have two parts that is away from each other during normal use, and only close to each other when the battery shall be charged.

    To get a high efficency the physical design of those parts must be optimized so the inductors are placed very close to each other, and probably also a core need to be used. I think it's therefore not possible to use any "off-the shelf" products, but I might be wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to enrico.migchels

    Hi Enrico!

     

    Thank you for your answer.

     

    I'm sorry, but I was maybe clera enough with my question:

     

    I have a lot of experience with power supply designs in general with for examples DC/DC converts with all kind of topologies.

    What I want to do now is something that is similar to an inductive charger for an electrical toothbrush, menaing with one part that act as a "transmitter" but that are completly sealed and not possible to touch any electrical parts.

    The second part shall act as a "receiver" (toothbrush) and is also completly sealed.

     

    So, I will have two parts that is away from each other during normal use, and only close to each other when the battery shall be charged.

    To get a high efficency the physical design of those parts must be optimized so the inductors are placed very close to each other, and probably also a core need to be used. I think it's therefore not possible to use any "off-the shelf" products, but I might be wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • enrico.migchels
    0 enrico.migchels over 16 years ago in reply to e14 Contributor

    Hi Roger,

     

    Ok, it's clear. The design problem is not as big as you think. Just see the distance between transmitter (primary part of your flyback converter) and receiver (secondary part of flyback converter) as the air gap which is normally in the centerleg of the core construction. In your situation the airgap is distributed in both centerleg as return legs. This is no problem. Try to limit the wall thickness of the plastics and try to position the transmitter/reciever are accurate as possible. What you have to do is build a circuit on the primary side which detects the receiver part (increase of inductance). This is the challanging part. I would seek for cores used in planar transformers as they are very low in height and have huge cross sections.

     

    Best regards,

     

    Enrico Migchels

    Power Conversion Design Engineer

    Best - The Netherlands

    www.heliox.nl